NX I-deas 6.2 Windows Post Release Support Issues

 June 11, 2013


June 11, 2013 HP Workstation and NVIDIA Graphics News

Siemens PLM Software would like to announce that it has certified and fully supports NX I-deas 6.2 on HP Z820 Workstation running Windows 7 64.  This includes certification of the following graphics as well.

August 30, 2012 NVIDIA Graphics News on Lenovo Workstation

Siemens PLM Software would like to announce that it has certified and fully supports NX I-deas 6.2 using the following NVIDIA graphics option running Windows 7 32 bit, 64 bit and Windows XP32 SP3 and XP64 SP2.

This certification was done using a Lenovo Thinkstation E31, but it is also supported on  the S30, D30 and C30.

June 6, 2012 Lenovo Workstation News

Siemens PLM Software would like to announce that it has certified and fully supports NX I-deas 6.2 on the Lenovo Thinkpad W530 running Windows XP 32 SP3 and Windows 7 64 with the following graphics options:

        NVIDIA K1000M

 

Siemens PLM Software would like to announce that it has also certified and fully supports NX I-deas 6.2 on the Lenovo Thinkstation E31 Tower running Windows XP 32 SP3, Windows XP 64 SP2 and Windows 7 64 SP1 with the following graphics options:

 

April 4, 2012 Lenovo Workstation News

Siemens PLM Software would like to announce that it has certified and fully supports NX I-deas 6.2 on the Lenovo Thinkstation C30, S30 and D30 running Windows XP Professional SP3, Windows XP x64 SP2 and Windows 7 32 & 64bit Professional.