The Teamcenter Services Reference has been enhanced with improved descriptions for service operations and data structures. This documentation can be used with all Teamcenter releases because signatures and functionality of the service operations remain unchanged between releases. The new and updated reference documentation will be supplied as part of distribution image of future release of the Teamcenter. As the majority of improved documentation is applicable to prior releases, we are making this available on GTAC, and you can use it by following the guidelines mentioned below.
The API documentation is available for each of the supported client bindings (Java, C++, .NET). Choose the language appropriate documentation:
Teamcenter Release | Namespace or Package |
Teamcenter 2007 | _2007_01 |
Teamcenter 2007.1 | _2007_06 |
Teamcenter 2007.1 MP1 | _2007_09 |
Teamcenter 2007.1 MP2 | _2007_12 |
Teamcenter 2007.1 MP3 | _2008_03 |
Teamcenter 2007.1 MP4 | _2008_05 |
Teamcenter 2007.1 MP5 | _2008_12 |
Teamcenter 2007.1 MP6 | _2009_01 |
Teamcenter 2007.1 MP7 | _2009_04 |
Teamcenter 2007.1 MP8 | _2009_05 |
Teamcenter 2007.2 | _2010_02 |
Teamcenter 8.0 | _2008_06 |
Teamcenter 8.0.1 | _2009_06 |
Teamcenter 8.1 | _2009_10 |
Teamcenter 8.2 | _2010_04 |
Teamcenter 8.3 | _2010_09 |
Teamcenter 8.3.1 | _2011_02 |
Teamcenter 8.3.2 | _2011_05 |
Teamcenter 8.3.3 | _2011_12 |
Teamcenter 9.0 | _2011_06 |
Teamcenter 9.1 | _2012_02 |
Teamcenter 9.1.1 | _2012_06 |
In
reviewing this Teamcenter SOA documentation,
please keep in mind, Teamcenter services that begin with date ‘2011_06’
or
newer are generally not available in Teamcenter 8.3. In this documentation, you will see the namespace '2012_09’ that is reserved for a future release
and is not available in Teamcenter 9.1.1 or earlier releases. For
example, the com.teamcenter.services.strong.core._2012_02.DataManagement.bulkCreateObjects
service operation is introduced in the Teamcenter 9.1 release and is
included
in this documentation set, it is not available in Teamcenter 8.2. There
some
exceptions to this as some service operations are back-ported to older
releases.
If
the
Teamcenter installation has been patched it is possible that newer SOA
services may
be made available. Please apply soa_client.zip that is included with
the patch
to update the SOA library resources.
To
review
if newer services are made available in a given patch, please do the
following:
Java: Open the
respective TcSoa<servicename>.jar
file (with your favorite Zip utility) and review
‘com/Teamcenter/services/strong’ for available services.
C++: Review the
header folder structure in
soa_client/cpp/includes/cpp/include/Teamcenter/services/<servicename>
for
available services.
C#: Open
the respective TcSoa<servicename> resource in VS “Object
Browser”.