The main program index contains the following line after each program listing:
Download: Source FileClicking on this line retrieves the text of the corresponding source file.
After you select a file from the download line, use the File, Save As to save the file to your local directory.
You can download either a WinNT version of the library in WINZIP format or
a Unix version in compressed tar format.
To extract files from this tar file, rename it from _name_.exe to _name.tar.Z,
(Unless it is already has an extension of .tar.Z).
If you are using UNIX, uncompress it using UNIX uncompress command,
then use a command like: tar xvf _name_.tar to extract the contents of
the tar file. Compile all the files and link the main routine.
If you are using Windows NT, uncompress the tar.Z file using the Winzip
utility. To get a copy, goto www.winzip.com.