Solid Edge Constants Type Library : ApplicationGlobalConstants Enumeration |
Member | Value | Description |
---|---|---|
seApplicationGlobalActivateAllParts | 66 | |
seApplicationGlobalAdminFileLocation | 53 | AdminFileLocation |
seApplicationGlobalANSIInchToleranceFile | 97 | ANSI Inch Tolerance File |
seApplicationGlobalANSIMetricToleranceFile | 98 | ANSI Metric Tolerance File |
seApplicationGlobalApplicationDisplay | 18 | Application display mode for new windows |
seApplicationGlobalApplyActivationOverridesToParts | 65 | |
seApplicationGlobalApplySimplifyOverridesToParts | 67 | |
seApplicationGlobalApplySimplifyOverridesToSubAssemblies | 69 | |
seApplicationGlobalApplyStatusToLinks | 36 | Apply Status To Links |
seApplicationGlobalAutomaticSave | 12 | |
seApplicationGlobalAutomaticSaveTime | 13 | |
seApplicationGlobalAutoSharpenLevel | 110 | Automatic sharpen level |
seApplicationGlobalAvailableRootFolder | 39 | Available Root Folder |
seApplicationGlobalBaselinedRootFolder | 44 | Baselined Root Folder |
seApplicationGlobalChangedPartActivation | 140 | |
seApplicationGlobalCheckInOnClose | 20 | Check In On Close |
seApplicationGlobalColorActive | 2 | The color for active elements |
seApplicationGlobalColorBackground | 3 | The color for the background |
seApplicationGlobalColorConstruction | 4 | The color for construction elements |
seApplicationGlobalColorDisabled | 5 | The color for disabled items |
seApplicationGlobalColorFailed | 6 | The color for failed items |
seApplicationGlobalColorHandle | 7 | The color for handles |
seApplicationGlobalColorHighlight | 8 | The color for highlighted elements |
seApplicationGlobalColorLiveSectionCenterline | 92 | |
seApplicationGlobalColorLiveSectionEdge | 91 | |
seApplicationGlobalColorLiveSectionOpacity | 94 | |
seApplicationGlobalColorLiveSectionRegion | 93 | |
seApplicationGlobalColorManagerCopyIndividualFaceColors | 58 | |
seApplicationGlobalColorManagerShowAssemblyStyleOverrides | 57 | |
seApplicationGlobalColorManagerShowPartFaceColors | 56 | |
seApplicationGlobalColorManagerUseIndividualPartStyles | 55 | |
seApplicationGlobalColorManagerUseToolsOptionsColorSettings | 54 | |
seApplicationGlobalColorProfile | 9 | The color for profiles, sketches and layouts |
seApplicationGlobalColorRefPlane | 31 | |
seApplicationGlobalColorSelected | 10 | The color for items in the select set |
seApplicationGlobalColorSheet | 11 | The color for the sheet |
seApplicationGlobalColorSheetTab1 | 138 | Specifies the first of two alternating colors for the sheet tabs. |
seApplicationGlobalColorSheetTab2 | 139 | Specifies the second of two alternating colors for the sheet tabs. |
seApplicationGlobalCommandBarMode | 105 | Displays mode in command bar or quick bar. |
seApplicationGlobalCurvatureCombDensity | 34 | |
seApplicationGlobalCurvatureCombMagnitude | 35 | |
seApplicationGlobalCustomSettingFile | 63 | |
seApplicationGlobalDefaultSharpness | 19 | Default sharpness for new windows |
seApplicationGlobalDisplayArcQuality | 1 | |
seApplicationGlobalDisplayQuality | 0 | |
seApplicationGlobalDisplaySectionCaps | 15 | Enable the display of section caps with dynamic sections |
seApplicationGlobalDisplayStatistics | 14 | Enable display timing statistics in the status bar |
seApplicationGlobalDocumentNameFormula | 88 | |
seApplicationGlobalDynamicTransition | 17 | Dynamic view transition smoothness |
seApplicationGlobalECORootFolder | 50 | ECO Root Folder |
seApplicationGlobalECRRootFolder | 49 | ECR Root Folder |
seApplicationGlobalEnableDynamicTolerance | 45 | Enable dynamic tolerancing of facet data |
seApplicationGlobalEnableThreadedDisplay | 30 | Enable multithreaded displays |
seApplicationGlobalHideAllComponents | 64 | |
seApplicationGlobalHoleSizeFile | 61 | |
seApplicationGlobalInReviewRootFolder | 43 | In Review Root Folder |
seApplicationGlobalInsightCacheLocation | 22 | Set InsightCacheLocation |
seApplicationGlobalInsightFolderMappingFileLocation | 23 | Set InsightFolderMappingFileLocation |
seApplicationGlobalInWorkRootFolder | 41 | Obsolete Root Folder |
seApplicationGlobalISOToleranceFile | 99 | ISO Tolerance File |
seApplicationGlobalLogFilesLocation | 21 | Set LogFilesLocation |
seApplicationGlobalLookAheadVersion | 26 | LookAheadVersion |
seApplicationGlobalMakeRevisionsObsolete | 38 | Make Revisions Obsolete |
seApplicationGlobalObsoleteRootFolder | 40 | Obsolete Root Folder |
seApplicationGlobalOfflineMode | 25 | Set OfflineMode |
seApplicationGlobalOnLineHelpLocation | 144 | |
seApplicationGlobalOpacityRefPlane | 32 | |
seApplicationGlobalOpenAsReadOnly3DFile | 89 | |
seApplicationGlobalOpenAsReadOnly3DFile_IndirectFiles | 95 | |
seApplicationGlobalOpenAsReadOnlyDftFile | 90 | |
seApplicationGlobalOpenAsReadOnlyDftFile_IndirectFiles | 96 | |
seApplicationGlobalOverlayColor | 28 | The color for visible edge overlay |
seApplicationGlobalOverlayColorMode | 29 | The color mode for visible edge overlay [1=Absolute, 2=Relative] |
seApplicationGlobalPackagedCollaborationRootFolder | 48 | Packaged Collaboration Root Folder |
seApplicationGlobalPipeThreadfsFile | 62 | |
seApplicationGlobalPrereleaseRootFolder | 47 | Prerelease Root Folder |
seApplicationGlobalReleasedRootFolder | 42 | Released Root Folder |
seApplicationGlobalRevisionDelimiter | 33 | Sets Revision Delimiter |
seApplicationGlobalSaveMultiCADDatasettoTC | 135 | |
seApplicationGlobalSearchScope | 24 | Set SearchScope |
seApplicationGlobalSectionCurvatureCombDensity | 141 | |
seApplicationGlobalSectionCurvatureCombMagnitude | 142 | |
seApplicationGlobalSessionDraftOpenInactive | 60 | Draft inactive mode on open (boolean) |
seApplicationGlobalSheetTabDisplayInfo | 136 | Specifies what information is displayed in the sheet tab : 0 = sheet number; 1 = sheet name; 2 = sheet number and sheet name |
seApplicationGlobalSheetTabDisplayInfoSeparator | 137 | Specifies the separator string used between the sheet number and sheet name when both are displayed in the sheet tabs. |
seApplicationGlobalShowUnitsInValueFields | 104 | Shows units of measure in value fields. |
seApplicationGlobalSoftwareVHL | 16 | Enable software VHL/Disable hardware VHL |
seApplicationGlobalStatusBarCmdFinder | 84 | Status Bar Command Finder |
seApplicationGlobalStatusBarCommonViews | 78 | Status Bar Common Views |
seApplicationGlobalStatusBarFit | 73 | Status Bar Fit |
seApplicationGlobalStatusBarLookAtFace | 77 | Status Bar Look At Face |
seApplicationGlobalStatusBarNamedViews | 80 | Status Bar Named Views |
seApplicationGlobalStatusBarPan | 74 | Status Bar Pan |
seApplicationGlobalStatusBarPreviousView | 79 | Status Bar Previous View |
seApplicationGlobalStatusBarRecordVideo | 145 | |
seApplicationGlobalStatusBarRotateView | 75 | Status Bar Rotate View |
seApplicationGlobalStatusBarSketchView | 86 | Status Bar Sketch View |
seApplicationGlobalStatusBarSpinAbout | 76 | Status Bar Spin About |
seApplicationGlobalStatusBarUploadToYouTube | 146 | |
seApplicationGlobalStatusBarViewStyles | 81 | Status Bar View Styles |
seApplicationGlobalStatusBarZoom | 71 | |
seApplicationGlobalStatusBarZoomArea | 72 | Status Bar Zoom Area |
seApplicationGlobalStatusBarZoomSlider | 82 | Status Bar Zoom Slider |
seApplicationGlobalStatusBarZoomTool | 83 | Status Bar Zoom Tool |
seApplicationGlobalSystemInfo | 46 | Retrieve system information [readonly] |
seApplicationGlobalTeamcenterFormula | 87 | |
seApplicationGlobalTeamCenterMode | 59 | |
seApplicationGlobalTemplateRootFolder | 51 | |
seApplicationGlobalUpdateDraft | 37 | Update draft files also |
seApplicationGlobalUploadOnClose | 27 | Upload On Close |
seApplicationGlobalUseAllSimplifiedParts | 68 | |
seApplicationGlobalUseAllSimplifiedSubAssemblies | 70 | |
seApplicationGlobalUseDetailEnvelopeDisplayAsCircle | 102 | Show Detail Envelope as Circle when TRUE. |
seApplicationGlobalUseDetailEnvelopeStandard | 101 | Use to set the Detail Envelope Standard Constants. Valid values are defined by enum DetailEnvelopeStandardConstants. |
seApplicationGlobalUseDimensionStyleElementMapAngularCoordinateDim | 118 | |
seApplicationGlobalUseDimensionStyleElementMapAngularDim | 117 | |
seApplicationGlobalUseDimensionStyleElementMapBalloon | 123 | |
seApplicationGlobalUseDimensionStyleElementMapBHC | 122 | |
seApplicationGlobalUseDimensionStyleElementMapBlockLabels | 134 | |
seApplicationGlobalUseDimensionStyleElementMapCallouts | 124 | |
seApplicationGlobalUseDimensionStyleElementMapCenterline | 120 | |
seApplicationGlobalUseDimensionStyleElementMapCenterMark | 121 | |
seApplicationGlobalUseDimensionStyleElementMapChamferDim | 119 | |
seApplicationGlobalUseDimensionStyleElementMapCircularDiameterDim | 114 | |
seApplicationGlobalUseDimensionStyleElementMapConnectors | 126 | |
seApplicationGlobalUseDimensionStyleElementMapCoordinateDim | 116 | |
seApplicationGlobalUseDimensionStyleElementMapDatumFrames | 130 | |
seApplicationGlobalUseDimensionStyleElementMapDatumPoints | 131 | |
seApplicationGlobalUseDimensionStyleElementMapDatumTargets | 132 | |
seApplicationGlobalUseDimensionStyleElementMapEdgeCondition | 129 | |
seApplicationGlobalUseDimensionStyleElementMapFCF | 133 | |
seApplicationGlobalUseDimensionStyleElementMapLeaders | 125 | |
seApplicationGlobalUseDimensionStyleElementMapLinDim | 111 | |
seApplicationGlobalUseDimensionStyleElementMapRadialDiameterDim | 113 | |
seApplicationGlobalUseDimensionStyleElementMapRadialDim | 112 | |
seApplicationGlobalUseDimensionStyleElementMapSTSymbols | 127 | |
seApplicationGlobalUseDimensionStyleElementMapSymmetricDiameterDim | 115 | |
seApplicationGlobalUseDimensionStyleElementMapWeldSymbols | 128 | |
seApplicationGlobalUseDimensionStyleMapping | 52 | |
seApplicationGlobalUseDrawingViewShowCroppingEdges | 103 | Show cropping edges when TRUE. |
seApplicationGlobalUseDrawingViewShowEdgesHiddenTangentEdgesHiddenByOtherParts | 107 | Show tangent edges that are hidden by other parts when TRUE. |
seApplicationGlobalUseDrawingViewShowEdgesHiddenTangentEdgesSelfHidden | 106 | Show the hidden tangent edges when TRUE. |
seApplicationGlobalUseISOToleranceTable | 100 | Use ISO Tolerance Table when TRUE. Use ANSI Tolerance Table when FALSE. |
seApplicationGlobalUseOnLineHelp | 143 | |
seApplicationGlobalUserType | 85 | Global User Type |
seApplicationGlobalZebraFolderMapping | 109 | Set ZebraFolderMapping |
seApplicationGlobalZebraFormula | 108 |
Solid Edge ST5 - What's New | Solid Edge ST4 - What's New | Solid Edge ST4 MP8 - What's New | Solid Edge ST3 - What's New | Solid Edge ST2 - What's New | Solid Edge ST - What's New | Solid Edge V20 - What's New | Solid Edge V19 - What's New | Solid Edge V18 - What's New | Solid Edge V18 SP4 - What's New | Solid Edge V17 - What's New