Solid Edge Draft Type Library
DetailEnvelopeStandardConstants Enumeration
Description
Enumerates the standards used to display the detail envelope.
Members
MemberValueDescription
seDetailEnvelopeANSI0The ANSI standard, the caption is embedded within the detail envelope.
seDetailEnvelopeESKD2The ESKD standard, the caption is displayed below the detail envelope. A leader line connects the caption to the detail envelope.
seDetailEnvelopeISO1The ISO standard, the caption is displayed below the detail envelope.
See Also

Solid Edge ST2 - What's New

Send comments on this topic.