Solid Edge FrameworkSupport Type Library
AnnotAlignmentShape Object
Members 
Description
This class is for handling individual 'AnnotAlignmentShape'.
Object Model
AnnotAlignmentShape ObjectApplication ObjectSelectSet CollectionAddIns CollectionApplication ObjectApplicationEvents ObjectApplicationV8DocumentOpenEvent ObjectApplicationWindowEvents ObjectCommand ObjectCustomization ObjectDocuments CollectionEnvironments CollectionFeatureLibraryEvents ObjectFileUIEvents ObjectMatTable ObjectInsight ObjectNewFileUIEvents ObjectApplication ObjectSEECEvents ObjectShortcutMenuEvents ObjectSolidEdgeInsightXT ObjectSolidEdgeTCE ObjectWindows Collection
Example
Imports System.Runtime.InteropServices
Public Class AnnotAlignmentShape
    Private Sub btnAnnotAlignmentShape_Click(sender As System.Object, e As System.EventArgs) Handles btnAnnotAlignmentShape.Click
        Dim objApplication As SolidEdgeFramework.Application = Nothing
        Dim objLine As SolidEdgeFrameworkSupport.Line2d = Nothing
        Dim objCircle As SolidEdgeFrameworkSupport.Circle2d = Nothing
        Dim objDraftDoc As SolidEdgeDraft.DraftDocument = Nothing
        Dim objAlignmentShape As SolidEdgeFrameworkSupport.AnnotAlignmentShape = Nothing
        Dim objType As Type = Nothing
        Dim DrawingView As SolidEdgeDraft.DrawingView = Nothing
        Dim DrawingViews As SolidEdgeDraft.DrawingViews = Nothing
        Dim DrawingView1 As SolidEdgeDraft.DrawingView = Nothing
        Dim balloons As SolidEdgeFrameworkSupport.Balloons = Nothing
        Dim balloon As SolidEdgeFrameworkSupport.Balloon = Nothing
        Dim itemNumberDir As SolidEdgeFrameworkSupport.DimItemNumDirConstants = Nothing
        Dim objFirstballoon As SolidEdgeFrameworkSupport.Balloon = Nothing
        Dim nIndex As Integer
        Dim PointX As Double
        Dim PointY As Double
        Dim objSheet As SolidEdgeDraft.Sheet = Nothing
        Dim objAnnotAlignmentShapes As SolidEdgeFrameworkSupport.AnnotAlignmentShapes = Nothing
        Dim objAnnotAlignmentShape As SolidEdgeFrameworkSupport.AnnotAlignmentShape = Nothing
        Dim dPointX(0 To 5) As Double
        Dim dPointY(0 To 5) As Double
        Dim bClosedAlignmentShape As Boolean
        Dim bUniformSpacing As Boolean
        Dim bMinimumSpacing As Boolean
        Dim dMinimumSpacingValue As Double
        Dim dPointX1(0 To 5) As Double
        Dim dPointY1(0 To 5) As Double
        Dim dPointX2(0 To 5) As Double
        Dim dPointY2(0 To 5) As Double
        Dim nVertexCount As Integer

        Try
            ' Create/get the application with specific settings
            objApplication = Marshal.GetActiveObject("SolidEdge.Application")

            If objApplication Is Nothing Then
                ' Get the type from the Solid Edge ProgID
                objType = Type.GetTypeFromProgID("SolidEdge.Application")
                ' Start Solid Edge
                objApplication = Activator.CreateInstance(objType)
                ' Make Solid Edge visible
                objApplication.Visible = True
            End If
            'Get reference to active document
            objDraftDoc = objApplication.ActiveDocument
            'Get reference to sheet
            objSheet = objDraftDoc.ActiveSheet

            'Populate array for x-coordinate of points of Annotation Alignment Shape
            dPointX(0) = 0.0
            dPointX(1) = 0.1
            dPointX(2) = 0.1
            dPointX(3) = 0.0
            dPointX(4) = 0.0
            'Populate array for y-coordinate of points of Annotation Alignment Shape
            dPointY(0) = 0.0
            dPointY(1) = 0.0
            dPointY(2) = 0.1
            dPointY(3) = 0.1
            dPointY(4) = 0.0

            objAnnotAlignmentShapes = objSheet.AnnotAlignmentShapes
            'Add balloon in the sheet
            balloons = objSheet.Balloons
            balloon = balloons.Add(0.1, 0.1, 0)
            balloon.Leader = True
            balloon.AddVertex(0.1, 0.1, 0)

            ' for AddAnnotAlignmentShape and other properties specific to alignment shapes.
            objAnnotAlignmentShape = objAnnotAlignmentShapes.AddAnnotAlignmentShape(dPointX, dPointY)

            Call balloon.SetAlignmentShape(objAnnotAlignmentShape, 0.05, 0.0)
            Call balloon.GetAlignmentShape(objAlignmentShape, PointX, PointY)

            'TRUE If the Annotation Alignment Shape is closed
            bClosedAlignmentShape = objAnnotAlignmentShape.ClosedAlignmentShape
            'Set value for Uniform Spacing
            objAnnotAlignmentShape.UniformSpacing = True
            bUniformSpacing = objAnnotAlignmentShape.UniformSpacing
            objAnnotAlignmentShape.MinimumSpacing = True
            bMinimumSpacing = objAnnotAlignmentShape.MinimumSpacing
            'Set value for Minimum Spacing
            objAnnotAlignmentShape.MinimumSpacingValue = 0.05
            dMinimumSpacingValue = objAnnotAlignmentShape.MinimumSpacingValue

            'Get X and Y coordinates of Annotation Alignment Shape
            objAnnotAlignmentShape.GetGeometry(dPointX1, dPointY1)
            'Get Number of vertes of Annotation Alignment Shape
            nVertexCount = objAnnotAlignmentShape.VertexCount
            'Insert vertex point in Annotation Alignment Shape
            objAnnotAlignmentShape.InsertVertex(0.05, 0.0)
            'Remove vertex point from Annotation Alignment Shape
            objAnnotAlignmentShape.RemoveVertex(2)
            'Modify vertex point from Annotation Alignment Shape
            objAnnotAlignmentShape.ModifyVertex(1, 0.1, 0.0)

            balloons = objSheet.Balloons
            DrawingViews = objSheet.DrawingViews
            objAnnotAlignmentShapes = objSheet.AnnotAlignmentShapes

            DrawingView = DrawingViews.Item(1)

            objAnnotAlignmentShape = objAnnotAlignmentShapes.Item(1)

            DrawingView1 = objAnnotAlignmentShape.DrawingView

            'Set and get item number direction
            objAnnotAlignmentShape.ItemNumberDirection = SolidEdgeFrameworkSupport.DimItemNumDirConstants.igDimItemNumberDirectionClockwise

            itemNumberDir = objAnnotAlignmentShape.ItemNumberDirection

            ' Set and get first balloon
            objFirstballoon = objAnnotAlignmentShape.FirstBalloon

            nIndex = objFirstballoon.Index

            objAnnotAlignmentShape.FirstBalloon = balloons.Item(2)

            'Dim DrawingView1 As SolidEdgeDraft.DrawingView

            objSheet = objDraftDoc.ActiveSheet
            DrawingViews = objSheet.DrawingViews
            DrawingView = DrawingViews.Item(1)

            ' for set and get alignment drawing view
            objAnnotAlignmentShape.DrawingView = DrawingView
            DrawingView1 = objAnnotAlignmentShape.DrawingView

        Catch ex As Exception
            MsgBox(ex.ToString)
        End Try
    End Sub

End Class
See Also

AnnotAlignmentShape Members

Send comments on this topic.