Solid Edge FrameworkSupport Type Library
Balloon Object
Members 
Description
An annotation object that consists of text contained within a closed shape.
Object Model
Balloon ObjectApplication ObjectSelectSet CollectionAddIns CollectionApplication ObjectApplicationEvents ObjectApplicationV8DocumentOpenEvent ObjectApplicationWindowEvents ObjectCommand ObjectCustomization ObjectDocuments CollectionEnvironments CollectionFeatureLibraryEvents ObjectFileUIEvents ObjectMatTable ObjectInsight ObjectNewFileUIEvents ObjectApplication ObjectSEECEvents ObjectShortcutMenuEvents ObjectSolidEdgeInsightXT ObjectSolidEdgeTCE ObjectWindows CollectionDisplayData ObjectDimStyle Object
Remarks
The Balloon object is an annotation object that consists of text contained within a closed shape. A Balloon object can be customized and manipulated through its properties and methods. For example, the shape of the balloon, breakline characteristics, orientation, and so forth can be set to meet specific requirements or preferences.
Example
Imports System.Runtime.InteropServices



Public Class AddBalloonCallOutLeader

    Private Sub Form1_Load(sender As System.Object, e As System.EventArgs) Handles MyBase.Load
        Dim objApplication As SolidEdgeFramework.Application = Nothing
        Dim objDraftDocument As SolidEdgeDraft.DraftDocument = Nothing
        Dim objSheet As SolidEdgeDraft.Sheet = Nothing
        Dim objBalloons As SolidEdgeFrameworkSupport.Balloons = Nothing
        Dim objBall As SolidEdgeFrameworkSupport.Balloon = Nothing

        Try
            objApplication = GetObject(, "SolidEdge.Application")
            objApplication.Visible = True
            objDraftDocument = objApplication.ActiveDocument
            objSheet = objDraftDocument.ActiveSheet
            objBalloons = objSheet.Balloons

            'Following Code will add Balloon in the sheet

            objBall = objBalloons.Add(0.05, 0.05, 0)
            objBall.TextScale = 1.0
            objBall.BalloonText = "B"
            objBall.Leader = True
            objBall.BreakLine = True
            objBall.BalloonSize = 3
            objBall.SetTerminator(objBall, 0, 0, 0, False)
            objBall.BalloonType = SolidEdgeFrameworkSupport.DimBalloonTypeConstants.igDimBalloonCircle
            objBall.Style.TerminatorType = SolidEdgeFrameworkSupport.DimTermTypeConstants.igDimStyleTermFilled 'Change Terminator Type if reqd

            'Following Code will add Callout in the sheet

            objBall = objBalloons.Add(0.1, 0.1, 0)
            objBall.Callout = True
            objBall.TextScale = 1.0
            objBall.BalloonText = "This is a Callout"
            objBall.Leader = True
            objBall.BreakLine = True
            objBall.BalloonSize = 3
            objBall.SetTerminator(objBall, 0, 0, 0, False)
            objBall.BalloonType = SolidEdgeFrameworkSupport.DimBalloonTypeConstants.igDimBalloonCircle
            objBall.Style.TerminatorType = SolidEdgeFrameworkSupport.DimTermTypeConstants.igDimStyleTermFilled 'Change Terminator Type if reqd

            Marshal.ReleaseComObject(objBall) : objBall = Nothing
            Marshal.ReleaseComObject(objSheet) : objSheet = Nothing
            Marshal.ReleaseComObject(objDraftDocument) : objDraftDocument = Nothing

        Catch ex As Exception
            Console.WriteLine(ex.ToString)
        End Try
    End Sub

End Class

See Also

Balloon Members

Send comments on this topic.