Solid Edge FrameworkSupport Type Library
Boundary2d Object
Members 
Description
Represents a closed 2-D region.
Object Model
Boundary2d ObjectApplication ObjectSelectSet CollectionAddIns CollectionApplication ObjectApplicationEvents ObjectApplicationV8DocumentOpenEvent ObjectApplicationWindowEvents ObjectCommand ObjectCustomization ObjectDocuments CollectionEnvironments CollectionFeatureLibraryEvents ObjectFileUIEvents ObjectMatTable ObjectInsight ObjectNewFileUIEvents ObjectApplication ObjectSEECEvents ObjectShortcutMenuEvents ObjectSolidEdgeInsightXT ObjectSolidEdgeTCE ObjectWindows CollectionBoundingObjects2d CollectionBoundaryStyle2d Object
Remarks
Displays with a solid fill or hatch fill style. The region is defined by a single outer shape and can contain multiple inner shapes that define holes in the region. Boundary2d objects can be created using the methods on the Boundaries2d collection object. The geometry of the Boundary2d object can be driven by a list of related linear geometrical elements (such as lines, arcs, and circles) that define a closed region. The BoundingObjects2d collection object provides access to the related linear geometrical elements. The Boundary2d display is controlled by a Fill Style that can provide a solid fill or a hatch fill. The display characteristics of a Boundary2d object can be overridden using the methods and properties on the BoundaryStyle2d object.
See Also

Boundary2d Members

Send comments on this topic.