Solid Edge FrameworkSupport Type Library
BoundaryStyle2d Object
Members 
Description
Provides properties and methods that allow you to change the Fill Style or to override the display characteristics of a Boundary2d object.
Remarks
The Style property on the Boundary2d object returns a BoundaryStyle2d object. The FillName property on BoundaryStyle2d object returns the name of the current fill style or assigns a new fill style to the Boundary2d object. The remaining properties set and return the current display characteristics (line color and width, for example) of the related Boundary2d object.
See Also

BoundaryStyle2d Members

Send comments on this topic.