Solid Edge FrameworkSupport Type Library
CenterLine Object
Members 
Description
A linear element that delineates the center of a nonlinear object.
Object Model
CenterLine ObjectApplication ObjectSelectSet CollectionAddIns CollectionApplication ObjectApplicationEvents ObjectApplicationV8DocumentOpenEvent ObjectApplicationWindowEvents ObjectCommand ObjectCustomization ObjectDocuments CollectionEnvironments CollectionFeatureLibraryEvents ObjectFileUIEvents ObjectMatTable ObjectInsight ObjectNewFileUIEvents ObjectApplication ObjectSEECEvents ObjectShortcutMenuEvents ObjectSolidEdgeInsightXT ObjectSolidEdgeTCE ObjectWindows CollectionDimStyle Object
Remarks
The characteristics of the centerline are determined by the active dimension style settings. That is, the current active width and line type determines the line width and style, respectively.
See Also

CenterLine Members

Send comments on this topic.