Solid Edge FrameworkSupport Type Library
DimStyle Object
Members 
Description
A virtual object on a specific dimension.
Remarks
The properties for this object can be set to override the associated dimension style for individual objects. These properties are defined on an object-by-object basis. That is, each object initially receives the property values defined by the DimensionStyle object and thus is customized by modifying the DimStyle properties.
See Also

DimStyle Members

Send comments on this topic.