Solid Edge FrameworkSupport Type Library
Dimension Object
Members 
Description
Stores characteristics such as size, distance, and angle.
Object Model
Dimension ObjectApplication ObjectSelectSet CollectionAddIns CollectionApplication ObjectApplicationEvents ObjectApplicationV8DocumentOpenEvent ObjectApplicationWindowEvents ObjectCommand ObjectCustomization ObjectDocuments CollectionEnvironments CollectionFeatureLibraryEvents ObjectFileUIEvents ObjectMatTable ObjectInsight ObjectNewFileUIEvents ObjectApplication ObjectSEECEvents ObjectShortcutMenuEvents ObjectSolidEdgeInsightXT ObjectSolidEdgeTCE ObjectWindows CollectionDisplayData ObjectDimStyle Object
Remarks
The dimensioning objects are associative to the geometry they are measuring. The Dimension object is created only through the Dimensions collection object.
See Also

Dimension Members

Send comments on this topic.