Solid Edge FrameworkSupport Type Library
FilletGeometry2d Object
Members 
Description
Contains methods and properties for an Arc2d object defined as a fillet.
Remarks
The GetConnectedObjects method on this object returns the two objects being filleted. All other properties of the fillet are edited by changing the properties of the Arc2d object.
See Also

FilletGeometry2d Members

Send comments on this topic.