Solid Edge FrameworkSupport Type Library
GeometryStyle2d Object
Members 
Description
Controls geometric characteristics for 2-D geometry objects.
Remarks
The characteristics are set or retrieved through the methods and properties associated with the GeometryStyle2d object. Characteristics set through these methods and properties apply only to the 2-D geometrical object that owns the GeometryStyle2d object.
See Also

GeometryStyle2d Members

Send comments on this topic.