Solid Edge FrameworkSupport Type Library
Relation2d Object
Members 
Description
Controls the graphic behavior of one or more graphic objects.
Object Model
Relation2d ObjectApplication ObjectSelectSet CollectionAddIns CollectionApplication ObjectApplicationEvents ObjectApplicationV8DocumentOpenEvent ObjectApplicationWindowEvents ObjectCommand ObjectCustomization ObjectDocuments CollectionEnvironments CollectionFeatureLibraryEvents ObjectFileUIEvents ObjectMatTable ObjectInsight ObjectNewFileUIEvents ObjectApplication ObjectSEECEvents ObjectShortcutMenuEvents ObjectSolidEdgeInsightXT ObjectSolidEdgeTCE ObjectWindows Collection
Remarks
For example, a Relation2d object whose type is igHorizontalRelation2d will insure that its related line is horizontal. One whose type is igPerpendicularRelation2d will insure that two elements remain perpendicular.
See Also

Relation2d Members

Send comments on this topic.