Solid Edge FrameworkSupport Type Library
SmartFrame2dStyle Object
Members 
Description
Holds properties to be used to determine the behavior of a SmartFrame2d object.
Object Model
SmartFrame2dStyle ObjectApplication ObjectSelectSet CollectionAddIns CollectionApplication ObjectApplicationEvents ObjectApplicationV8DocumentOpenEvent ObjectApplicationWindowEvents ObjectCommand ObjectCustomization ObjectDocuments CollectionEnvironments CollectionFeatureLibraryEvents ObjectFileUIEvents ObjectMatTable ObjectInsight ObjectNewFileUIEvents ObjectApplication ObjectSEECEvents ObjectShortcutMenuEvents ObjectSolidEdgeInsightXT ObjectSolidEdgeTCE ObjectWindows CollectionSmartFrame2dDefaults ObjectFrame Object
Remarks
Many of the properties are used only by commands that create and manipulate a Smart Frame. These commands are not used by the SmartFrame2d object internally. The BehaviorDefaults property returns an object that contains a list of properties that are not reapplied to the SmartFrame2d after seeding it the first time. (That is, if these properties change, objects that used the properties are not changed.)
See Also

SmartFrame2dStyle Members

Send comments on this topic.