Solid Edge FrameworkSupport Type Library
SurfaceFinishSymbolDataSets Collection
Members 
Description
A collection of SurfaceFinishSymbolDataSet objects.
Remarks
Each of these collections of settings is a data set. By adding a data set to the SurfaceFinishSymbolDataSets collection object, those settings are available to the SurfaceFinishSymbols collection object as a DataSet property. This property specifies the set of surface finish symbol characteristics on which to base a new SurfaceFinishSymbol object.
See Also

SurfaceFinishSymbolDataSets Members

Send comments on this topic.