Solid Edge FrameworkSupport Type Library
WeldSymbol Object
Members 
Description
Specifies all unique weld types necessary in the fabrication of the weldment.
Object Model
WeldSymbol ObjectApplication ObjectSelectSet CollectionAddIns CollectionApplication ObjectApplicationEvents ObjectApplicationV8DocumentOpenEvent ObjectApplicationWindowEvents ObjectCommand ObjectCustomization ObjectDocuments CollectionEnvironments CollectionFeatureLibraryEvents ObjectFileUIEvents ObjectMatTable ObjectInsight ObjectNewFileUIEvents ObjectApplication ObjectSEECEvents ObjectShortcutMenuEvents ObjectSolidEdgeInsightXT ObjectSolidEdgeTCE ObjectWindows CollectionDisplayData ObjectDimStyle Object
Remarks
The characteristics of the weld (such as the top and bottom treatment types) conveyed by the weld symbol are controlled by the properties of the WeldSymbol object.
See Also

WeldSymbol Members

Send comments on this topic.