Solid Edge FrameworkSupport Type Library
WeldSymbolDataSets Collection
Members 
Description
A collection of WeldSymbolDataSet objects.
Remarks
Each of these collection of settings is a data set. By adding a data set to the WeldSymbolDataSets collection object, those settings are available to the WeldSymbols collection object as a DataSet property selection. This property specifies the set of surface finish symbol characteristics on which to base a new WeldSymbol object.
See Also

WeldSymbolDataSets Members

Send comments on this topic.