Solid Edge FrameworkSupport Type Library
WeldSymbols Collection
Members 
Description
A collection of WeldSymbol objects.
Remarks
WeldSymbol objects that are created through this collection receive the current dimension, text, and surface finish symbol property settings. The default values can be applied to these objects by using the ClearStyle or ClearDataSet methods before adding the object to the collection. In addition, the DataSet property can be specified before adding the new WeldSymbol object to retrieve the weld symbol characteristics on which the new object is to be based.
See Also

WeldSymbols Members

Send comments on this topic.