Solid Edge Part Type Library
BodyFeature Object
Members 
Description
Represents the base feature object in the Features object collection, if a non Solid Edge file is opened in Solid Edge.
Object Model
BodyFeature ObjectApplication ObjectSelectSet CollectionAddIns CollectionApplication ObjectApplicationEvents ObjectApplicationV8DocumentOpenEvent ObjectApplicationWindowEvents ObjectCommand ObjectCustomization ObjectDocuments CollectionEnvironments CollectionFeatureLibraryEvents ObjectFileUIEvents ObjectMatTable ObjectInsight ObjectNewFileUIEvents ObjectApplication ObjectSEECEvents ObjectShortcutMenuEvents ObjectSolidEdgeInsightXT ObjectSolidEdgeTCE ObjectWindows CollectionFaceStyle ObjectSuppressVariable ObjectApplication Object
See Also

BodyFeature Members

Send comments on this topic.