Solid Edge Part Type Library
CloseCorner Object
Members 
Description
An occurrence of a CloseCorner feature in a Sheet Metal part.
Object Model
CloseCorner ObjectApplication ObjectSelectSet CollectionAddIns CollectionApplication ObjectApplicationEvents ObjectApplicationV8DocumentOpenEvent ObjectApplicationWindowEvents ObjectCommand ObjectCustomization ObjectDocuments CollectionEnvironments CollectionFeatureLibraryEvents ObjectFileUIEvents ObjectMatTable ObjectInsight ObjectNewFileUIEvents ObjectApplication ObjectSEECEvents ObjectShortcutMenuEvents ObjectSolidEdgeInsightXT ObjectSolidEdgeTCE ObjectWindows CollectionFaceStyle ObjectSuppressVariable ObjectApplication Object
Example
Imports System.IO
Imports System.Runtime.InteropServices

Module Example
    <STAThread()> _
    Sub Main()
        Dim objApplication As SolidEdgeFramework.Application = Nothing
        Dim objDocuments As SolidEdgeFramework.Documents = Nothing
        Dim objSheetmetalDocument As SolidEdgePart.SheetMetalDocument = Nothing
        Dim objModels As SolidEdgePart.Models = Nothing
        Dim objModel As SolidEdgePart.Model = Nothing
        Dim objFlanges As SolidEdgePart.Flanges = Nothing
        Dim objFlange1 As SolidEdgePart.Flange = Nothing
        Dim objFlange2 As SolidEdgePart.Flange = Nothing
        Dim objFaces As SolidEdgeGeometry.Faces = Nothing
        Dim objFace As SolidEdgeGeometry.Face = Nothing
        Dim objEdges1 As SolidEdgeGeometry.Edges = Nothing
        Dim objEdges2 As SolidEdgeGeometry.Edges = Nothing
        Dim objEdge1 As SolidEdgeGeometry.Edge = Nothing
        Dim objEdge2 As SolidEdgeGeometry.Edge = Nothing
        Dim objCornerEdge As SolidEdgeGeometry.Edge = Nothing
        Dim objCloseCorners As SolidEdgePart.CloseCorners = Nothing
        Dim objCloseCorner As SolidEdgePart.CloseCorner = Nothing
        Dim i As Long
        Dim j As Long
        Dim bFound As Boolean
        Dim dOffsetValue As Double
        Dim RefLayer As Long

        Try
            OleMessageFilter.Register()

            ' Start Solid Edge
            objApplication = Activator.CreateInstance(Type.GetTypeFromProgID("SolidEdge.Application"))
            objApplication.Visible = True
            objDocuments = objApplication.Documents

            'Any sheet metal document contains more two flanges
            objSheetmetalDocument = objDocuments.Open("anyfilename.psm")

            objModels = objSheetmetalDocument.Models
            objModel = objModels.Item(1)
            objFlanges = objModel.Flanges
            objFlange1 = objFlanges(1)
            objFlange2 = objFlanges(2)
            objEdges1 = objFlange1.Edges(SolidEdgeGeometry.FeatureTopologyQueryTypeConstants.igQueryAll)
            objEdges2 = objFlange2.Edges(SolidEdgeGeometry.FeatureTopologyQueryTypeConstants.igQueryAll)

            bFound = False
            For i = 0 To objEdges1.Count
                objEdge1 = objEdges1(i + 1)
                For j = 0 To objEdges2.Count
                    objEdge2 = objEdges2(j + 1)
                    If (objEdge1 Is objEdge2) Then
                        bFound = True
                        objCornerEdge = objEdge1
                        Exit For
                    End If
                Next j
                If bFound Then
                    Exit For
                End If
            Next i

            If bFound <> True Then
                Throw New System.Exception("Could not find the appropriate close corner edge.")
            End If

            'Got it, go ahead to create close corner feature
            objCloseCorners = objModel.CloseCorners
            If objCloseCorners Is Nothing Then
                Throw New System.Exception("Could not get the close corner collect.")
            End If

            ' use the default value to create a simple corner
            objCloseCorner = objCloseCorners.Add(objCornerEdge)

        Catch ex As Exception
            Console.WriteLine(ex.Message)
        Finally
            OleMessageFilter.Revoke()
        End Try
    End Sub
End Module
See Also

CloseCorner Members

Send comments on this topic.