Solid Edge Part Type Library
CrossCurve Object
Members 
Description
Represents an occurrence of a CrossCurve feature in a Part document.
Object Model
CrossCurve ObjectApplication ObjectSelectSet CollectionAddIns CollectionApplication ObjectApplicationEvents ObjectApplicationV8DocumentOpenEvent ObjectApplicationWindowEvents ObjectCommand ObjectCustomization ObjectDocuments CollectionEnvironments CollectionFeatureLibraryEvents ObjectFileUIEvents ObjectMatTable ObjectInsight ObjectNewFileUIEvents ObjectApplication ObjectSEECEvents ObjectShortcutMenuEvents ObjectSolidEdgeInsightXT ObjectSolidEdgeTCE ObjectWindows CollectionSuppressVariable ObjectApplication Object
Remarks
The CrossCurve object represents an occurrence of a curve generated from the intersection of the projections of two specified curves.
See Also

CrossCurve Members

Send comments on this topic.