Solid Edge Part Type Library
FamilyMember Object
Members 
Description
Represents an occurrence of a Family of Parts member in a Part or Sheet Metal document.
Object Model
FamilyMember ObjectApplication ObjectSelectSet CollectionAddIns CollectionApplication ObjectApplicationEvents ObjectApplicationV8DocumentOpenEvent ObjectApplicationWindowEvents ObjectCommand ObjectCustomization ObjectDocuments CollectionEnvironments CollectionFeatureLibraryEvents ObjectFileUIEvents ObjectMatTable ObjectInsight ObjectNewFileUIEvents ObjectApplication ObjectSEECEvents ObjectShortcutMenuEvents ObjectSolidEdgeInsightXT ObjectSolidEdgeTCE ObjectWindows Collection
Example
Imports System.IO
Imports System.Runtime.InteropServices

Module Example
    <STAThread()> _
    Sub Main()
        Dim objApplication As SolidEdgeFramework.Application = Nothing
        Dim objPartDocument As SolidEdgePart.PartDocument = Nothing
        Dim objFamilyMembers As SolidEdgePart.FamilyMembers = Nothing
        Dim objFamilyMember As SolidEdgePart.FamilyMember = Nothing

        Try
            OleMessageFilter.Register()

            ' Connect to Solid Edge
            objApplication = Marshal.GetActiveObject("SolidEdge.Application")
            objApplication.Visible = True
            objPartDocument = objApplication.ActiveDocument
            objFamilyMembers = objPartDocument.FamilyMembers

            ' Loop through famliy members.
            For Each objFamilyMember In objFamilyMembers

            Next
        Catch ex As Exception
            Console.WriteLine(ex.Message)
        Finally
            OleMessageFilter.Revoke()
        End Try
    End Sub
End Module
See Also

FamilyMember Members

Send comments on this topic.