Solid Edge Part Type Library
Hole Object
Members 
Description
A type of cutout that uses a circular pattern.
Object Model
Hole ObjectApplication ObjectSelectSet CollectionAddIns CollectionApplication ObjectApplicationEvents ObjectApplicationV8DocumentOpenEvent ObjectApplicationWindowEvents ObjectCommand ObjectCustomization ObjectDocuments CollectionEnvironments CollectionFeatureLibraryEvents ObjectFileUIEvents ObjectMatTable ObjectInsight ObjectNewFileUIEvents ObjectApplication ObjectSEECEvents ObjectShortcutMenuEvents ObjectSolidEdgeInsightXT ObjectSolidEdgeTCE ObjectWindows CollectionFaceStyle ObjectSuppressVariable ObjectApplication Object
Remarks
This feature is a type of cutout that always uses a circular profile. Additionally, the Hole object contains substantial feature attribute information (HoleData information) to allow for generative machining directly from the definition of the hole(s).
See Also

Hole Members

Send comments on this topic.