Solid Edge Part Type Library
ModelingModeConstants Enumeration
Description
Modeling mode for the referenced object.
Members
MemberValueDescription
seModelingModeOrdered2Ordered mode (traditional)
seModelingModeSynchronous1Synchronous mode
Remarks
Each object in the Features collection, where appropriate, will have a new read-only property, ModelingModeType, that will distinguish it between Synchronous and Ordered. Methods/Properties not appropriate for a given ModelingModeType will return CO_E_NOT_SUPPORTED.
Example
Imports System.IO
Imports System.Runtime.InteropServices

Module Example
    <STAThread()> _
    Sub Main()
        Dim objApplication As SolidEdgeFramework.Application = Nothing
        Dim objSolidEdgeDocument As SolidEdgeFramework.SolidEdgeDocument = Nothing
        Dim objModels As SolidEdgePart.Models = Nothing
        Dim objModel As SolidEdgePart.Model = Nothing
        Dim objFeatures As SolidEdgePart.Features = Nothing
        Dim objFeature As Object = Nothing

        Try
            OleMessageFilter.Register()

            objApplication = Marshal.GetActiveObject("SolidEdge.Application")
            objSolidEdgeDocument = objApplication.ActiveDocument

            Select Case objSolidEdgeDocument.Type
                Case SolidEdgeFramework.DocumentTypeConstants.igPartDocument
                    objModels = objSolidEdgeDocument.Models
                Case SolidEdgeFramework.DocumentTypeConstants.igSheetMetalDocument
                    objModels = objSolidEdgeDocument.Models
            End Select

            If Not objModels Is Nothing Then
                objModel = objModels.Item(1)
                objFeatures = objModel.Features

                ' Loop through all the features of the model.
                For Each objFeature In objFeatures
                    Select Case objFeature.ModelingModeType
                        Case SolidEdgePart.ModelingModeConstants.seModelingModeOrdered
                            ' Ordered feature.
                        Case SolidEdgePart.ModelingModeConstants.seModelingModeSynchronous
                            ' Synchronous feature.
                    End Select
                Next
            End If
        Catch ex As Exception
            Console.WriteLine(ex.Message)
        Finally
            OleMessageFilter.Revoke()
        End Try
    End Sub
End Module
See Also

Solid Edge ST3 - What's New

Send comments on this topic.