Solid Edge Part Type Library
Count Property
Description
Returns the number of objects in the referenced collection.
Property type
Read-only property
Syntax
Visual Basic
Public Property Count As Long
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objEPProfile As SolidEdgePart.Profile
    Dim objEPProfArray(1 To 2) As SolidEdgePart.Profile
    Dim objEPModel As SolidEdgePart.Model
    Dim objRPProfile As SolidEdgePart.Profile
    Dim objRPProfArray(1 To 2) As SolidEdgePart.Profile
    Dim objRPLine As SolidEdgeFrameworkSupport.Line2d
    Dim objRPRAxis As SolidEdgePart.RefAxis
    Dim objRPCSection As SolidEdgeFrameworkSupport.Circle2d
    Dim objRPModel As SolidEdgePart.Model
    Dim lngStatus As Long
    Dim lngCount As Long
    ' Report errors
    Const PI = 3.14159265358979
    ' Create/get the application with specific settings
    On Error Resume Next
    Set objApp = GetObject(, "SolidEdge.Application")
    If Err Then
        Err.Clear
        Set objApp = CreateObject("SolidEdge.Application")
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    ' *** creating the first model
    ' creating the profile for an extruded protrusion feature
    Set objEPProfile = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:=objDoc.RefPlanes(1))
    Call objEPProfile.Circles2d.AddByCenterRadius(x:=0, y:=0, Radius:=0.025)
    lngStatus = objEPProfile.End(ValidationCriteria:=igProfileClosed)
    If (lngStatus <> 0) Then
        MsgBox "Profile for the base feature is not closed"
    End If
    objEPProfile.Visible = False
    ' creating the base extruded protrusion
    Set objEPProfArray(1) = objEPProfile
    Set objEPModel = objDoc.Models.AddFiniteExtrudedProtrusion(NumberOfProfiles:=1, _
                                                               ProfileArray:=objEPProfArray, ProfilePlaneSide:=igSymmetric, _
                                                               ExtrusionDistance:=0.1)
    If (objEPModel.ExtrudedProtrusions(1).Status <> igFeatureOK) Then
        MsgBox "AddFiniteExtrudedProtrusion method fails"
    End If
    ' *** creating the second model
    ' creating a reference axis and a cross-section for a revolved protrusion feature
    Set objRPProfile = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:=objDoc.RefPlanes(2))
    Set objRPLine = objRPProfile.Lines2d.AddBy2Points(x1:=0, y1:=-0.05, x2:=0, y2:=0.05)
    Set objRPRAxis = objRPProfile.SetAxisOfRevolution(lineforaxis:=objRPLine)
    Set objRPCSection = objRPProfile.Circles2d.AddByCenterRadius(x:=0.1, y:=0, Radius:=0.025)
    lngStatus = objRPProfile.End(ValidationCriteria:=igProfileNoSelfIntersect)
    If lngStatus <> 0 Then
        MsgBox "Profile for the revolved protrusion is self-intersecting"
    End If
    objRPProfile.Visible = False
    ' creating the base revolved protrusion
    Set objRPProfArray(1) = objRPProfile
    Set objRPModel = objDoc.Models.AddFiniteRevolvedProtrusion(NumberOfProfiles:=1, _
                                                               ProfileArray:=objRPProfArray, ReferenceAxis:=objRPRAxis, _
                                                               ProfilePlaneSide:=igRight, AngleOfRevolution:=3 * PI / 2)
    ' getting the number of model objects in the models collection
    lngCount = objDoc.Models.Count
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objEPProfile = Nothing
    Set objEPProfArray(1) = Nothing
    Set objEPModel = Nothing
    Set objRPProfile = Nothing
    Set objRPLine = Nothing
    Set objRPRAxis = Nothing
    Set objRPProfArray(1) = Nothing
    Set objRPCSection = Nothing
    Set objRPModel = Nothing
End Sub
See Also

Models Collection  | Models Members

Send comments on this topic.