Solid Edge Part Type Library
RevolvedCutout Object
Members 
Description
A feature that is defined by using an open or closed profile that revolves about a reference axis.
Object Model
RevolvedCutout ObjectApplication ObjectSelectSet CollectionAddIns CollectionApplication ObjectApplicationEvents ObjectApplicationV8DocumentOpenEvent ObjectApplicationWindowEvents ObjectCommand ObjectCustomization ObjectDocuments CollectionEnvironments CollectionFeatureLibraryEvents ObjectFileUIEvents ObjectMatTable ObjectInsight ObjectNewFileUIEvents ObjectApplication ObjectSEECEvents ObjectShortcutMenuEvents ObjectSolidEdgeInsightXT ObjectSolidEdgeTCE ObjectWindows CollectionFaceStyle ObjectSuppressVariable ObjectApplication Object
Remarks
A Revolved Cutout feature is defined using an open or closed profile that revolves about a Reference Axis (a RefAxis object). The volume that is defined by the revolution is removed from the solid.
See Also

RevolvedCutout Members

Send comments on this topic.