Solid Edge Part Type Library
Thinwall Object
Members 
Description
Represents an occurrence of a Thinwall feature in a Part document.
Object Model
Thinwall ObjectApplication ObjectSelectSet CollectionAddIns CollectionApplication ObjectApplicationEvents ObjectApplicationV8DocumentOpenEvent ObjectApplicationWindowEvents ObjectCommand ObjectCustomization ObjectDocuments CollectionEnvironments CollectionFeatureLibraryEvents ObjectFileUIEvents ObjectMatTable ObjectInsight ObjectNewFileUIEvents ObjectApplication ObjectSEECEvents ObjectShortcutMenuEvents ObjectSolidEdgeInsightXT ObjectSolidEdgeTCE ObjectWindows CollectionFaceStyle ObjectSuppressVariable ObjectApplication Object
Remarks
A Thinwall is a solid feature that is constructed by clearing a volume from a part, leaving a solid shell. Any features that are placed on the Thinwall object at the time that the Thinwall object is created automatically inherit the common thickness of the part. A new Thinwall object cannot be created for features that are added to a part after the creation of the initial Thinwall object. If a feature is reordered to occur before the Thinwall operation was performed, it will be included in the Thinwall operation.
See Also

Thinwall Members

Send comments on this topic.