Solid Edge Part Type Library
Union Object
Members 
Description
Object Model
Union ObjectApplication ObjectSelectSet CollectionAddIns CollectionApplication ObjectApplicationEvents ObjectApplicationV8DocumentOpenEvent ObjectApplicationWindowEvents ObjectCommand ObjectCustomization ObjectDocuments CollectionEnvironments CollectionFeatureLibraryEvents ObjectFileUIEvents ObjectMatTable ObjectInsight ObjectNewFileUIEvents ObjectApplication ObjectSEECEvents ObjectShortcutMenuEvents ObjectSolidEdgeInsightXT ObjectSolidEdgeTCE ObjectWindows CollectionFaceStyle ObjectSuppressVariable ObjectApplication Object
Example
Imports System.IO
Imports System.Runtime.InteropServices

Module Example
    <STAThread()> _
    Sub Main()
        Dim objApplication As SolidEdgeFramework.Application = Nothing
        Dim objPartDocument As SolidEdgePart.PartDocument = Nothing
        Dim objModels As SolidEdgePart.Models = Nothing
        Dim objModel As SolidEdgePart.Model = Nothing
        Dim objUnions As SolidEdgePart.Unions = Nothing
        Dim objUnion As SolidEdgePart.Union = Nothing
        Dim objTargetBodyunion(5) As Object
        Dim objToolBodyunion(5) As Object

        Try
            OleMessageFilter.Register()

            objApplication = Marshal.GetActiveObject("SolidEdge.Application")
            objPartDocument = objApplication.ActiveDocument

            ' get the Model collection
            objModels = objPartDocument.Models

            objTargetBodyunion(0) = objModels.Item(1).Body
            objToolBodyunion(0) = objModels.Item(2).Body
            objToolBodyunion(1) = objModels.Item(3).Body
            objToolBodyunion(2) = objModels.Item(4).Body

            objModel = objModels.Item(1)
            objUnions = objModel.Unions
            objUnion = objUnions.Item(1)

        Catch ex As Exception
            Console.WriteLine(ex.Message)
        Finally
            OleMessageFilter.Revoke()
        End Try
    End Sub
End Module
See Also

Union Members  | Solid Edge ST5 - What's New

Send comments on this topic.