Imports RevisionManager
Imports System.Runtime.InteropServices
Module Example
Sub Main()
Dim objApplication As RevisionManager.Application = Nothing
Dim objInsight As RevisionManager.Insight = Nothing
Dim ServerFileUrl As String
Dim bIsSpssupported As Boolean
Try
' Start Revision Manager.
objApplication = New RevisionManager.Application
' Get reference to Insight object.
objInsight = objApplication.Insight
ServerFileUrl = "D:\InsightCache\Insight\solidvm\Engineering\PreReleased\PreReleasedDocLib\Summit.par"
' Check if the current versions of solid edge and sharepoint are compatible.
objInsight.CheckSupport(ServerFileUrl, bIsSpssupported)
If (bIsSpssupported) Then
' File is supported.
End If
Catch ex As Exception
' Write any errors to console.
Console.WriteLine(ex.Message)
Finally
' Release COM Objects.
If Not (objInsight Is Nothing) Then
Marshal.ReleaseComObject(objInsight)
objInsight = Nothing
End If
If Not (objApplication Is Nothing) Then
objApplication.Quit()
Marshal.ReleaseComObject(objApplication)
objApplication = Nothing
End If
End Try
End Sub
End Module