--------------
Legal Notices
--------------
©2010 Siemens Product Lifecycle Management Software Inc.
All Rights Reserved
Software, file formats, and audiovisual displays may be used pursuant to the
applicable Software License Agreement and contain confidential and proprietary
information of Siemens Product Lifecycle Management Software Inc.; which is
protected by copyright and trade secret law. Such materials may not be reproduced
or transferred to other documents or used or disclosed to others for manufacturing
or for any other purpose except as specifically authorized within the terms of the
Software License Agreement, or as specifically authorized in writing by Siemens
Product Lifecycle Management Software Inc.
Siemens Product Lifecycle Management Software Inc.
5800 Granite Parkway
Suite 600
Plano, TX. 75024
--------------------
End of Legal Notices
--------------------
--------------
Release Notes:
--------------
Product: Solid Edge
Version: 102.00.11.03
Date: 17-Dec-2010
Maintenance Packs are all inclusive and can be installed on top of the base
release or any released Maintenance Pack.
This Maintenance Pack can be installed on top of Versions:
102.00.00.116, 102.00.01.04, 102.00.02.06, 102.00.03.04. 102.00.04.03, 102.00.05.04,
102.00.06.04, 102.00.07.04, 102.00.08.04, 102.00.09.05, or 102.00.10.04.
This release of Solid Edge has been certified to run on the following:
- Windows XP Professional© operating system (32-bit or 64-bit)
- Windows Vista Business© or Vista Enterprise© operating system (32-bit or 64-bit)
- Windows 7 Professional©, Enterprise©, or Ultimate© operating system (32-bit or 64-bit)
- Internet Explorer 7 or 8 (IE 6.0 minimum)
User Account Control (UAC) -- Due to continued reports of problems with Solid Edge installation and removal, Solid Edge licensing, Insight web parts and other cases writing to text files in the program folder, it is recommended that the UAC be turned off when running on Windows 7 or Vista.
Windows 7: Control Panel -> User Accounts -> Change User Account Control settings ->
Never notify
Vista: Control Panel -> User Accounts and Family Safety -> User Accounts ->
Turn User Account Control Off.
--------------------
End of Release Notes
--------------------
-------------------
Installation Notes:
-------------------
After downloading the Maintenance Pack to your machine, dbl click the downloaded
file and the Maintenance Pack will install.
-------------------
End of Installation
-------------------
--------------------------------------------------
This Maintenance Pack addresses the following PRs:
--------------------------------------------------
===API===
PR 2153824: Japanese text input in a custom property is garbled
=====Assembly=====
PR 1811489: Display performance problem in assembly after activating a part
PR 1814714: Assembly-Driven Part Features are failing after suppress / unsuppress
PR 1815082: abort while assembling parts
PR 1818652: Edges are left in original location after Move Faces
PR 6436398: Material Table not updating from Solid Edge Admin
PR 6437662: When the provided JT file is opened in Solid Edge the product aborts
PR 6446125: crashing in docking pane interaction (via submitted crashlogs)
=====Draft=====
PR 1809132: Constraint handles printing
PR 1808576: Sheet contents disappeared - Please Repair in ST2
PR 1810175: Crash during Replace Block
PR 6411077: Parts list copy to clipboard format is different for reverse order of entries
PR 6422866: copy/paste of drawing views
PR 6440087: Copy/paste doesn't work
PR 1807028: Translate Part layer names as AutoCAD layer names results in blank file names
===Insight/View & Markup===
PR 1799833: Error Exception in Models object when running in Insight environment
PR 6413940: Property Manager displaying values in the wrong fields
PR 6433729: Opening assembly brings down the wrong parts associated with sub assemblies
PR 6397983: Rev Manager is not resolving last opened file location in Set Path dialog
PR 6414056: Create Insight Full Text Index incorrectly adds -t 7608 switch to SQL Server
=====Part/Profile/Sheet Metal=====
PR 1778645: Draft face analysis settings are not correct, compared to ST
PR 1808975: Cannot include elements in a sketch
PR 1812196: flat pattern fails
PR 1814007: Pattern is not symmetric to the center of the part
PR 6222922: Copy-Paste-Attach of Flange and Drawn cutout problem
PR 6271173: Unable to attach detached drawn cutout on a partial flange
PR 6450991: PMI Dimension Display - Font Smoothing
===== Solid Edge Embedded Client=====
PR 2155011: Smart Codes do not recognize name rule for custom Item type
PR 6416470: "From linked 3D" does not copy the properties from linked file to the draft
PR 6426239: Please add the new CheckBOMStructure API
PR 1796494: Custom Item Name is not preserved during a Save As from Structure Editor
PR 6434610: Edits to variables are taking entirely too much time compared to unmanaged edits
PR 6427105: User can checkout a file on two computers at the same time
---
End
---