--------------
Legal Notices
--------------
©2011 Siemens Product Lifecycle Management Software Inc.
All Rights Reserved
Software, file formats, and audiovisual displays may be used pursuant to the
applicable Software License Agreement and contain confidential and proprietary
information of Siemens Product Lifecycle Management Software Inc.; which is
protected by copyright and trade secret law. Such materials may not be reproduced
or transferred to other documents or used or disclosed to others for manufacturing
or for any other purpose except as specifically authorized within the terms of the
Software License Agreement, or as specifically authorized in writing by Siemens
Product Lifecycle Management Software Inc.
Siemens Product Lifecycle Management Software Inc.
5800 Granite Parkway
Suite 600
Plano, TX. 75024
--------------------
End of Legal Notices
--------------------
--------------
Release Notes:
--------------
Product: Solid Edge
Version: 103.00.04.05
Date: 08-Apr-2011
Maintenance Packs are all inclusive and can be installed on top of the base
release or any released Maintenance Pack.
This Maintenance Pack can be installed on top of Versions:
103.00.00.114, 103.00.01.05, 103.00.02.04, or 103.00.03.04
This release of Solid Edge has been certified to run on the following:
- Windows XP Professional operating system (32-bit or 64-bit)
- Windows Vista Business or Vista Enterprise operating system (32-bit or 64-bit)
- Windows 7 Enterprise, Ultimate and Professional (32-bit or 64-bit)
- Internet Explorer 8 (IE 6.0 meets minimum requirements)
Please see the Solid Edge Readme file (Readme.htm) in the ...\Program Files\Solid Edge ST3
folder for additional details.
--------------------
End of Release Notes
--------------------
-------------------
Installation Notes:
-------------------
After downloading the Maintenance Pack to your machine, dbl click the downloaded
file and the Maintenance Pack will install.
-------------------
End of Installation
-------------------
--------------------------------------------------
This Maintenance Pack addresses the following PRs:
--------------------------------------------------
===Assembly===
PR 1833635: Web Publisher result are incorrect if a part has sync and ordered features
PR 1832106: Copied sketch elements, linked to the parent sketch, can be modified or deleted
PR 1835705: A crash occurs when a section view is applied and a part is placed
PR 2161686: Path dimensions disappearing in the frame environment.
PR 2163832: Assembly pathfinder losing display of icons and hide/show boxes
PR 2164176: Crash in XpresRoute when placing dimensions
PR 6426117: Fails to create Chamfer on Frame Pattern occurrence in first attempt
PR 6446233: Mirror assembly command fails with error message
PR 6459239: No user defined properties in assembly query
PR 6463932: Face of the flange should coincide with the endpoint of the line
PR 6471354: SAT file fails to import all bodies
PR 6484211: mass of frame components incorrect
PR 6382855: Change Source button is disabled in the Edit Links command
PR 6427250: pathfinder needs a lot of scroll in a particular workflow
PR 6472286: smart installer does not provide a way to not update already generated parts
PR 6450569: Crash on Right Click in Configuration Manager
PR 1823993: Offset value field disappears if more than one part is selected
PR 1834121: Unable to open X_T file in ST3
PR 1837775: Solid Edge hangs when selecting a link in pathfinder
PR 1840226: Cannot enter an offset distance of zero
PR 2164215: Unable to create spur gear as done in ST2
PR 6469288: 'Apply Configuration' dialog comes up, when applying subassembly configuration
PR 1838609: 'Center Distance Between' missing in Synchronous Pulley Designer
PR 6447436: the Select Identical Parts command not being available in ERA
===Draft===
PR 1827819: Property-text "Mass" (in draft) is empty, if drawing is opened without model
PR 1831283: Texture Symbols and Geo not imported
PR 1836610: Unable to save a single sheet to PDF to its correct size
PR 2097195: The space of the tolerance is too large
PR 6438504: Retrieve Dimensions will only work from one model at a time
PR 1830981: Parts list header text wrapping changed V20 vs. ST3
PR 1833476: Copy link / Paste special does not give correct result in ST3
PR 1836176: Draft where SE crashes in connection with 3D Device and mouse drag
PR 1836241: Parts list is not showing FOA member names
PR 1837622: Cannot open or create drawings after installing ST3 MP3
PR 6476574: sheet being renamed
PR 1840034: Performance problem updating views with PMI model views specified
PR 6439408: Bad Display in PDF
PR 6495446: Predefined Draft Text (Annotation) Alignment does not work
PR 1840906: SE aborts when updating view
PR 2166384: Leader display has changed from st2 to st3
PR 6461898: %RT does not work like it did in ST2
PR 6491943: Drawing view properties section tab not enabled/disabled based on PMI view selected
===Insight/View & Markup===
PR 6483466: Search not returning results from top level site only sub sites
PR 6484521: Crash saving as pdf into a DocLib with required properties
PR 6497333: Errors in Insight Logs since upgrading to MOSS2007/ST3
PR 6483575: FOA property mapping problems with SharePoint
===Part/Profile/Sheet Metal===
PR 1834162: Draft option in synchronous extrusion doesn’t work properly
PR 1824904: "Show only" is missing in ST3 ordered
PR 1832775: close corner reacts different in ST2
PR 1833282: Sheet metal local symmetry doesn’t work (Live Rules)
PR 6493372: Bend direction not showing on printed .psm documents from batch mode
PR 1835549: Unable to pattern a feature
PR 2164158: Extrude created a feature with a duplicate name
PR 6489351: Crash occurred while reorienting the steering wheel while in SE Simulation
PR 1838826: Dimensions placed with feature are not editable in FOP
PR 2165475: Japanese command tips being garbled in crashlogf.txt
PR 6493558: User is unable to scale a part copy when importing it into a new file
PR 1826580: It’s not possible to assign part material with ordered and synchronous features
PR 1829378: Material Thickness on Gage tab of File Properties dialog is no longer accessible
PR 1833358: feature library is not working
PR 1837948: Unable to flatten a psm file
PR 1838687: Solid Edge aborts when populating FOP members
PR 2165291: Normal Distance causes an abort in Japanese ST3 - Sync
PR 6385655: radial edits taking too long for synchronous models
PR 6389400: Wrong result on flat of conic shape with cutout
PR 6442323: cutout in ST3 synch part that takes 10-30 times as long as ordered
PR 1704478: After dissolving UDS, features don't remain selected
PR 1816608: smart pattern performance - applies to both pattern and pattern along curve
PR 1838985: Countersink is lost when re-bending
PR 2166692: Unable to select curve control points for connects with Solid Edge x64
PR 6461572: Pattern Plane creation is incorrect most of the time
PR 6469130: Product uses a lot of memory when placing sync cutout using Text Profile
PR 6509580: edit handle arrow does not point to edit face
===Solid Edge Embedded Client===
PR 6479486: SEEC API OnGetWhereUsedForAutomation does not work
PR 6495362: Unable to Check-in documents; returning document has moved or is missing error
PR 6507472: Need to verify the back port Item Number - Find No. Integration project
PR 6484387: No warning given for Item id conflicts with virtual components
PR 6512292: Next Available Number command doesn't consider TCVC
PR 6441245: Modified weldment feature is not updated in structure manager in RAC
PR 6471911: SEEC does not recognize multiple revisions during open in an assembly
PR 6482868: With PS_new_seqno_mode=none the Occurrence Properties show nothing
PR 6512110: after deleting assembly feature the JT is not updated in the Tc viewer
---
End
---