Solid Edge ST7 SDK
Solid Edge ST MP1 - Readme

--------------
Legal Notices
--------------
©2008 Siemens Product Lifecycle Management Software Inc.

All Rights Reserved
Software, file formats, and audiovisual displays may be used pursuant to the
applicable Software License Agreement and contain confidential and proprietary
information of Siemens Product Lifecycle Management Software Inc.; which is
protected by copyright and trade secret law. Such materials may not be reproduced
or transferred to other documents or used or disclosed to others for manufacturing
or for any other purpose except as specifically authorized within the terms of the
Software License Agreement, or as specifically authorized in writing by Siemens
Product Lifecycle Management Software Inc.

Siemens Product Lifecycle Management Software Inc.
5800 Granite Parkway
Suite 600
Plano, TX. 75024


--------------------
End of Legal Notices
--------------------

--------------
Release Notes:
--------------

Product:        Solid Edge
Version:        100.00.01.07
Date:           10-Oct-2008

This Maintenance Pack can be installed on top of Version: 100.00.00.133.

Note: Maintenance Packs are all inclusive and can be installed on top of the base
release or any released Maintenance Pack.

--------------------
End of Release Notes
--------------------

-------------------
Installation Notes:
-------------------

After downloading the Maintenance Pack to your machine, dbl click the downloaded
file and the Maintenance Pack will install.

-------------------
End of Installation
-------------------

--------------------------------------------------
This Maintenance Pack addresses the following PRs:
--------------------------------------------------

=====Assembly=====

PR 5969985: Fixed a problem to prevent crashes reported in auto-captured crashlogs.
PR 5943101: Fixed a problem that caused multiple JT crashes
PR 5899813: Fixed a problem where Solid Edge crashed when editing a weld label
PR 5872719: Fixed a problem where editing a Stitch Weld assembly feature causes an abort.
PR 1672958: Fixed a problem where answering NO to a Save As simplified overwrite prompt deletes the existing file.
PR 5987019: Fixed a problem where no bodies are created during import if imported files already exist in folder
PR 2082240: Fixed a problem where "Export Display Only" is not working when editing a sub-assembly
PR 5902637: Fixed a problem where Solid Edge crashes when opening a part from draft and in assembly.
PR 5842365: Fixed a problem where FOA conversion loses configuration files.
PR 2070584: Fixed a problem where a warning is not displayed when setting a part to inactive using configurations.
PR 5996894: Fixed a problem with view rotation performance.
PR 1599941: Fixed a problem where threaded holes in assembly have incorrect diameters.
PR 5997261: Fixed a problem where you cannot place PMI annotations while IPA in a sync assembly
PR 1674763: Fixed a problem where the match coordinate system command does not locate the coordinate system
PR 5999067: Fixed a problem where part key points are not locatable after placing a CS
PR 2104933: Fixed a problem where you cannot include normal to face using fence select
PR 6007266: Fixed a problem where Physical Property Manager doesn't display unassigned density dialog
PR 1676717: Fixed a problem where Rack and Pinion Gears Designer produces the wrong results
PR 1641424: Fixed a problem where Solid Edge crashes when working with zones or saving a file containing zones.
PR 5987105: Fixed a problem where Show/Hide is not working on Assembly groups.
PR 2105941: Fixed a problem where Solid Edge crashed using the "Explode" command.
PR 1594089: Fixed a problem where different end-conditions produce the same result on a frame. 
PR 1600542: Fixed a problem where deleted dim styles continue to show up in the template
PR 5874510: Fixed a problem where Solid Edge entered into a not responding state while simplifying assembly
PR 5737340: Fixed a problem where a circular dependency error is received using FlashFit.
PR 1545774: Fixed a problem where parts disappear during move when a section is active.
PR 6000268: Fixed a problem where orientating planes (n, b & t) fails in Traditional Assemblies
PR 2076104: Fixed a problem where the user is unable to auto-restore a backed up file.
PR 1649779: Fixed a problem where Solid Edge fires the wrong command ID when hitting DELETE key in assembly
PR 5999686: Fixed a problem where SmartStep is not appearing when switching from FlashFit to Axial Align.
PR 1628066: Fixed a problem with FOA and Assembly Features
PR 1668883: Fixed a problem where moving a part causes duplicate occurrences to be created in Edgebar
PR 5992055: Fixed a problem where you cannot fence locate when IPA – in Traditional
PR 6022024: Fixed a problem where include fails
PR 1510690: Fixed a problem where patterned parts are in the wrong position
PR 1681255: Fixed a problem where Save As Image does not create a rendered image in Foundation
PR 5834085: Fixed a problem where there is not a bolt for the given stack length.
PR 2088091: Fixed a problem where it takes more time and memory to update the "Physical Properties" than V18
PR 6016016: Fixed a problem where the assembly file reader does not work with sync assemblies
PR 2085635: Fixed a problem that caused Solid Edge to crash based on auto-captured crashlogs
PR 1610960: Fixed a problem where Frame components are not trimming correctly on all corners
PR 1586883: Fixed a problem where Part colors are not exported to step.
PR 5988839: Fixed a problem where Sub-assm reference planes turned ON after using Undo.
PR 6023710: Fixed a problem where washers are not available with a C'snk screw

=====Part=====

PR 5921066: Fixed a problem where hole callouts for patterned counterbores and countersinks are wrong in draft
PR 5999436: Fixed a problem where face-sets created by importing curves could not be deleted.
PR 5988541: Fixed a problem where Inter-Part Copy Option is not available in SYNC environment
PR 5985795: Fixed a problem where model geometry is not seen on opening new window for active document
PR 6004472: Fixed a problem where Solid Edge hangs when docking pane is unpinned
PR 6006019: Fixed a problem where Solid Edge crashes during the creation of a Helix
PR 6001450: Fixed a problem where Solid Edge crashes after a Hole placement error message
PR 6005555: Fixed a problem where Solid Edge crashes using the insert image command
PR 5771029: Fixed a problem where constraining a fixed pattern doesn't work properly
PR 5998249: Fixed a problem where associated occurrences are not removed when hole is deleted
PR 6003957: Fixed a problem where sketch geometry is not consumed by protrusion operation
PR 5998971: Fixed a problem where there is no shaded display for Acrylic High Density
PR 5986186: Fixed a problem where double clicking in pathfinder isn't expanding if you are IPA
PR 5988132: Fixed a problem where dimensions placed for a reference plane are driving dimensions
PR 5998262: Fixed a problem where you are unable to edit coordinate dimensions placed on sketch
PR 2084562: Fixed a problem where a Text Profile feature does not extend through part correctly
PR 6000298: Fixed a problem where you must place cursor over DEC and hit Esc twice to dismiss.
PR 5844833: Fixed a problem where a sheet metal part is displaying the wrong angle in draft
PR 6009190: Fixed a problem where Pattern Variables are not showing in Variable Table
PR 5991387: Change rectangular pattern from a 3-point rectangular back to 2-point rectangle in Traditional
PR 5986409: Fixed a problem where the Break Link Option is active for a sketch.
PR 6006526: Fixed a problem where Restore Sketch is removing all sketches from the file
PR 5986464: Fixed a problem where the Group option is active when in sketch environment
PR 6003104: Fixed a problem where an Undo error occurs after part document conversion to sync
PR 5989056: Fixed a problem selecting objects that are behind other objects in Sync parts and assemblies
PR 6014762: Fixed a problem where Solid Edge crashes after creating a Group and using "Measure Distance"
PR 6004169: Fixed a problem where Solid Edge crashes after hitting ESC key while editing a pattern
PR 5991849: Fixed a problem where additional context menu options active for simplify features.
PR 6020259: Fixed a problem where you cannot select a planar face/plane after using Hide Previous Level
PR 6018241: Fixed a problem where selecting a parting surface hangs Solid Edge
PR 6020895: Fixed a problem where you are unable to place some PMI dimensions in assembly
PR 1620911: Fixed a problem where convert to Sheet Metal operation fails
PR 6022795: Fixed a problem where user defined sets are not listed if they contain System defined face sets
PR 6024210: Fixed a problem where you can no longer attach a hole pattern on training part
PR 1641087: Fixed a problem where Solid Edge crashes using FOP with an old part
PR 2082794: Fixed a problem where an IGES file cannot be imported into ST if user login has double byte characters
PR 6006657: Fixed a problem where editing a dimension causes Solid Edge to shutdown because of low memory
PR 1668197: Fixed a problem where DIN.PZL will not be used for lofted flanges
PR 6020529: Fixed a problem where Solid Edge crashes after selecting a model view in part pathfinder
PR 6018317: Fixed a problem where Solid Edge crashes when placing a pattern in Sync part
PR 6019224: Fixed a problem where you are unable to reset the HOLES.TXT file location to a server location.
PR 1682195: Fixed a problem where separating a hole changes its diameter
PR 5993031: Fixed a problem where a view disappears while sketching a line
PR 6013504: Fixed a problem where some faces in the model do not belong to a face-set
PR 6006751: Fixed a problem where the Hole Table is not listing the correct hole diameter for a counterbore
PR 6005614: Fixed a problem where a pattern does not update after moving
PR 6027721: Fixed a problem where you can only move one side of a sync part regardless of move arrow direction
PR 5610929: Fixed a problem where Copy/Paste of Text Profile is not fully constrained like parent.
PR 6032804: Fixed a problem where the Dissolve User Defined Set command does not work.
PR 6025031: Fixed a problem where the provided assembly will not save to STL format.

=====Draft=====

PR 5999896: Fixed a problem where explode flow lines did not display immediately after placement of a view.
PR 1666634: Fixed a problem where a table style that is based on another style could not be edited.
PR 2104940: Fixed a problem where hidden layers were not hidden after drawing view converted to 2D.
PR 1561801: Fixed a problem where hardware parts were shown even when they did not intersect the cutting plane.
PR 6004783: Fixed a problem where dimension values double on broken 2D views.
PR 5982657: Fixed a problem where importing a Microstation 2-D dgn file causes Solid Edge to crash
PR 2103557: Fixed a problem where Blocks are not exporting to dxf on Japanese XP.
PR 1670678: Fixed a problem where Line width to ACAD Color mapping does not work for dimensions
PR 6000417: Fixed a problem where you cannot exit a Block edit using close button.
PR 6000905: Fixed a problem where opening a DGN file causes Solid Edge to abort
PR 1593505: Fixed a problem where Solid Edge crashed when deleting a symbol with bottom-up locate
PR 5991964: Fixed a problem where "Error: no reference" displayed in callouts linked to missing properties
PR 5990835: Fixed a problem where Solid Edge aborts after repeatedly updating views
PR 5971763: Fixed a problem where you are unable to Copy/Move multiple elements in Draw in View. 
PR 1619152: Fixed a problem where a drawing border is not saved out in pdf
PR 1632537: Fixed a problem where save as a pdf rotates the output from a draft file.
PR 5841236: Fixed a problem where zooming with Ctrl+RMB deselects geometry
PR 1616825: Fixed a problem where hitting the number 5 on the numeric key pad selects Endpoint
PR 1603406: Fixed a problem with performance when mirroring grouped elements in a draft-view
PR 1656622: Fixed a problem where an image is disappearing after pasting into Draft.
PR 1585174: Fixed a problem where Blocks were being placed corrupted.
PR 5992242: Fixed a problem where EMF's are scaled incorrectly
PR 1535069: Fixed a problem where you are unable to hide edge segments
PR 5421845: Fixed a problem where the font changes depending on how text box is selected
PR 5745434: Fixed a problem where a Block Name is not reflected in pathfinder if you undo after deleting
PR 1683721: Fixed a problem where you get incorrect dimension values to centermarks between views
PR 1625644: Fixed a problem where you cannot open specific Acad files
PR 6012783: Fixed a problem where a bitmap object regenerates on every display
PR 1659278: Fixed a problem where Open File -> AutoCAD documents -> causes Solid Edge to crash.
PR 5996870: Fixed a problem where the ACAD Wizard does not start for files with JPN characters in filename.
PR 2107915: Fixed a problem where data alignment in table properties is incorrect
PR 2105954: Fixed a problem where Japanese fonts are not mapped to ACAD fonts for export.
PR 6000242: Fixed a problem where you are unable to import an STL file.

=====API=====
 
PR 5999875: Fixed a problem where template names were truncated in the Application Menu
PR 6010963: Fixed a problem with Automation Commands Swept Surface, Revolved Surface and Extruded Surface issues.
PR 6010151: Fixed a problem where a few of the Automation APIs are not working for Sync Curves.
PR 6011974: Fixed a problem where a few Automation APIs are not working for Sync surfaces
PR 6016486: Fixed a problem where the Toolbar sample does not work properly
PR 2103667: Fixed a problem where the Symbol ConvertToGroup API is leaving geometry out of shape
PR 6012518: Fixed a problem where the Mirror API is not working
PR 6011839: Fixed a problem where 'SetOrientation' fails on a Sync Coordinate System.

=====Insight=====
 
PR 1675808: Fixed a problem where Revision Manager crashes when searching for broken Links on Hebrew OS.
PR 5991256: Fixed a problem where you are unable to change Doc No and Rev No in Rev Mgr for certain parts.
PR 5941829: Fixed a problem where revising Draft and FOP members are not updating everything in Rev Mgr
PR 5549874: Fixed a problem where parts are shown as Designed when the Simplified parts option is used.
PR 6020447: Fixed a problem where Rev Mgr gets in a loop when setting these files to Copy with Update Links
PR 6029411: Fixed a problem that caused Solid Edge to crash when IPA on a part or assembly file from Draft.
PR 5706206: Fixed a problem where Insight warnings appear for each file when saving assy.

---
End
---