--------------
Legal Notices
--------------
©2009 Siemens Product Lifecycle Management Software Inc.
All Rights Reserved
Software, file formats, and audiovisual displays may be used pursuant to the
applicable Software License Agreement and contain confidential and proprietary
information of Siemens Product Lifecycle Management Software Inc.; which is
protected by copyright and trade secret law. Such materials may not be reproduced
or transferred to other documents or used or disclosed to others for manufacturing
or for any other purpose except as specifically authorized within the terms of the
Software License Agreement, or as specifically authorized in writing by Siemens
Product Lifecycle Management Software Inc.
Siemens Product Lifecycle Management Software Inc.
5800 Granite Parkway
Suite 600
Plano, TX. 75024
--------------------
End of Legal Notices
--------------------
--------------
Release Notes:
--------------
Product: Solid Edge
Version: 100.00.10.05
Date: 09-Sep-2009
This Maintenance Pack can be installed on top of Versions:
100.00.00.133, 100.00.01.07, 100.00.02.07, 100.00.03.03, 100.00.04.04,
100.00.05.04, 100.00.06.03, 100.00.07.04, 100.00.08.03, 100.00.09.04
Note: Maintenance Packs are all inclusive and can be installed on top of the base
release or any released Maintenance Pack.
--------------------
End of Release Notes
--------------------
-------------------
Installation Notes:
-------------------
After downloading the Maintenance Pack to your machine, dbl click the downloaded
file and the Maintenance Pack will install.
-------------------
End of Installation
-------------------
--------------------------------------------------
This Maintenance Pack addresses the following PRs:
--------------------------------------------------
=====Assembly=====
PR 1722862: Fastener system does not work correctly, holes do not highlight as they did in V20
PR 6090914: Include command not working with maintain associativity off
PR 6168053: Cannot import the provided IGES file into Solid Edge Assembly
PR 6170573: Moving a face with multiple Coordinate Systems and the CS filter on, only moves one CS
PR 6184120: Right Mouse Button stops working
PR 6197873: Program Crashes (repeatedly) after Auto-saving
PR 6200343: Assembly relationships are not updating properly
PR 6180138: a phantom fitting is generated and cannot be deleted
PR 1743944: Opening document via API in hidden SE causes 100% processor time consumption
=====Part/Profile/Sheet Metal=====
PR 1729242: Sheetmetal Save As Flat, produces a DXF with incorrect line types
PR 6092467: Construction Names are not displayed in Draft View properties
PR 2105762: Round disappears when part is recomputed in Version20
PR 6061463: Dimensions that are placed between holes become sick
PR 1740832: Part Reference Planes are not updating when made coincident with assembly planes
=====Draft=====
PR 1727279: Can't switch on reference planes in PathFinder in sketch environment
PR 1730031: Received a message indicating that Viewer data cannot be stored
PR 1735692: Drafts will not print with "print all colors as black" option
PR 2105470: Surface lay symbol is not exported to DXF format
PR 6020435: Word document is not exporting to PDF
PR 1739896: Transparency is on for Inserted Images in Draft
PR 6210242: Solid Edge is crashing when opening this draft file
PR 1741068: dwg and dxf file cannot be opened - system runs out of memory
PR 2128278: Solid Edge crashes after inactivating part while in profile
PR 5996172: items on context menu in HyperLink command are disabled
===API===
PR 1675688: Solid Edge x64 crashes in LoftedSurfaces::Add
PR 6218347: Added API option to the SEReader.dll that will return the assembly
PR 1715979: StructuralFrames.Add fails with run-time error '5'
===Insight/View & Markup===
PR 1737834: SearchDuplicateIDs.exe doesn't report existing duplicates of SEDocIDs
PR 6191743: CFG files are remaining checked out and displayed in the Cache Assistant
PR 6215909: Revise of a subassembly leads to crash
PR 6216719: PCF file getting corrupted after opening twice then saving
PR 6217938: Show Revisions and Revised From commands don't work in Solid Edge Cache Assistant
=====Embedded Client=====
PR 1702749: Attribute map of TCstatus is incorrectly carry forward when file is revise
PR 6186436: 2-tier connection from Vista 64-bit returned 8004A0D0
PR 6191872: Update SEEC Overlay Template based on Tc8.0 MP1
PR 1742370: AddToTeamcenter, SEEC, and Structure Editor issues with long folder names in TcX/TcU
PR 1740376: SaveAs/Revise doesn't copy PDF datasets
PR 1742158: Attribute Problem with save as in SEEC
PR 6205376: after saving an assembly the resulting PSE BOM view is incomplete
---
End
---