Solid Edge ST7 SDK
Solid Edge ST MP12 - Readme

--------------
Legal Notices
--------------
©2009 Siemens Product Lifecycle Management Software Inc.

All Rights Reserved
Software, file formats, and audiovisual displays may be used pursuant to the
applicable Software License Agreement and contain confidential and proprietary
information of Siemens Product Lifecycle Management Software Inc.; which is
protected by copyright and trade secret law. Such materials may not be reproduced
or transferred to other documents or used or disclosed to others for manufacturing
or for any other purpose except as specifically authorized within the terms of the
Software License Agreement, or as specifically authorized in writing by Siemens
Product Lifecycle Management Software Inc.

Siemens Product Lifecycle Management Software Inc.
5800 Granite Parkway
Suite 600
Plano, TX. 75024


--------------------
End of Legal Notices
--------------------

--------------
Release Notes:
--------------

Product:        Solid Edge
Version:        100.00.12.03
Date:           13-Nov-2009

This Maintenance Pack can be installed on top of Versions: 100.00.00.133,
100.00.01.07, 100.00.02.07, 100.00.03.03, 100.00.04.04, 100.00.05.04,
100.00.06.03, 100.00.07.04, 100.00.08.03, 100.00.09.04, 100.00.10.05,
100.00.11.03

Note: Maintenance Packs are all inclusive and can be installed on top of the base
release or any released Maintenance Pack.

--------------------
End of Release Notes
--------------------

-------------------
Installation Notes:
-------------------

After downloading the Maintenance Pack to your machine, dbl click the downloaded
file and the Maintenance Pack will install.

-------------------
End of Installation
-------------------

--------------------------------------------------
This Maintenance Pack addresses the following PRs:
--------------------------------------------------

=====Assembly=====

PR 1727798: Cannot access Construction Display when creating a relationship
PR 1747914: XpresRoute piping automatically generates wrong Pipe-Segments
PR 6075333: Solid Edge Crash in Assembly
PR 6238380: Unable to open a top level assembly
PR 6208564: Solid Edge will crashes after rendering an image
PR 1754336: Grounded part can be moved, but should not
PR 6242272: performance enhancement for sketches in assembly

=====Part/Profile/Sheet Metal=====

PR 1745651: FEMAP date Patch
PR 1751696: SEPreview causes a crash
PR 6236238: Command Bar does not display correctly
PR 6244998: PMI dimension brackets are reversed in a model view
PR 2129612: Pattern parts not properly oriented when pattern along curve is used

=====Draft=====

PR 1689627: Material property not maintained when model not found
PR 1702644: Solid Edge crashes after undo on Broken out section
PR 1750199: line weights changing on copy and paste
PR 1751251: Dimensions between two drawing views are incorrect if the views have different origins
PR 1752285: Solid Edge Draft crashes in Convert to Geometry
PR 6240692: Ctrl-c not working in edit block environment
PR 6229622: Printing (or saving as PDF) causes shaded views to be blank
PR 1755493: DXF-export and wrong result
PR 1755536: Unable to set transparent color when inserting image

=====Embedded Client=====

PR 5772602: Unable to open files
PR 6244293: Add To Teamcenter dry-run will remove Document Number property values

---
End
---