Solid Edge ST7 SDK
Solid Edge ST MP13 - Readme

--------------
Legal Notices
--------------
©2010 Siemens Product Lifecycle Management Software Inc.

All Rights Reserved
Software, file formats, and audiovisual displays may be used pursuant to the
applicable Software License Agreement and contain confidential and proprietary
information of Siemens Product Lifecycle Management Software Inc.; which is
protected by copyright and trade secret law. Such materials may not be reproduced
or transferred to other documents or used or disclosed to others for manufacturing
or for any other purpose except as specifically authorized within the terms of the
Software License Agreement, or as specifically authorized in writing by Siemens
Product Lifecycle Management Software Inc.

Siemens Product Lifecycle Management Software Inc.
5800 Granite Parkway
Suite 600
Plano, TX. 75024


--------------------
End of Legal Notices
--------------------

--------------
Release Notes:
--------------

Product:        Solid Edge
Version:        100.00.13.03
Date:           22-Jan-2010

This Maintenance Pack can be installed on top of Versions: 100.00.00.133,
100.00.01.07, 100.00.02.07, 100.00.03.03, 100.00.04.04, 100.00.05.04,
100.00.06.03, 100.00.07.04, 100.00.08.03, 100.00.09.04, 100.00.10.05,
100.00.11.03, 100.00.12.03.

Note: Maintenance Packs are all inclusive and can be installed on top of the base
release or any released Maintenance Pack.

--------------------
End of Release Notes
--------------------

-------------------
Installation Notes:
-------------------

After downloading the Maintenance Pack to your machine, dbl click the downloaded
file and the Maintenance Pack will install.

-------------------
End of Installation
-------------------

--------------------------------------------------
This Maintenance Pack addresses the following PRs:
--------------------------------------------------

=====Assembly=====

PR 1762903: Unsuppress of a pattern was not recreating the slave parts
PR 2133252: Solid Edge ST MP10 aborts while trying to import an assembly from NX3.0
PR 6146834: Solid Edge is crashing while attempting to place fasteners
PR 6248060: Relationships failing when replacing a subassembly using same base part
PR 1702605: Parts have wrong position after replace part, but system gives no error
PR 6242099: Failed PMI dimension appears to dramatically affect performance in this assembly

=====Part/Profile/Sheet Metal=====

PR 1757659: Divide Part doesn't support rename of the child anymore - Regression
PR 2086784: Assembly section view is not cutting the body

=====Draft=====

PR 1753646: Abort occurred after entering invalid characters on the table style line type page
PR 2124797: Dimension changes when opened in V20
PR 2135361: a phantom sheet showing up in Draft file
PR 6234965: Pasting into a Feature Control Frame causes Solid Edge to abort
PR 1715016: Dimension values will not move, when the Drawing View is moved, regression against V19
PR 6276308: Solid Edge is crashing during Save after placing a connector, then deleting it

===Insight===

PR 6270672: Solid Edge crashes if you close the Search dialog before list refreshes
PR 6270698: Solid Edge crashes if you click Search before the old list is processed
PR 1759457: Copy alternate assemblies inherits wrong member

===API===

PR 6268536: SEReader failing to open Assembly locked by Solid Edge
PR 6272116: Heap overwrite detected when 3dConexion add-in is running

=====Embedded Client=====

PR 1754089: Assembly structure links are broken with "Hide all Components"
PR 1754460: PSE BOM doesn`t synchronize although "SEEC_BOM_Synchronize=TRUE"
PR 5937465: Error message, "Checked out by Another User" when downloading files from Cache Assistant
PR 6199990: Synchronize All in pathfinder does not update BOM changes
PR 6213940: Improved SEEC search time performance


---
End
---