Solid Edge ST7 SDK
Solid Edge ST MP2 - Readme

--------------
Legal Notices
--------------
©2008 Siemens Product Lifecycle Management Software Inc.

All Rights Reserved
Software, file formats, and audiovisual displays may be used pursuant to the
applicable Software License Agreement and contain confidential and proprietary
information of Siemens Product Lifecycle Management Software Inc.; which is
protected by copyright and trade secret law. Such materials may not be reproduced
or transferred to other documents or used or disclosed to others for manufacturing
or for any other purpose except as specifically authorized within the terms of the
Software License Agreement, or as specifically authorized in writing by Siemens
Product Lifecycle Management Software Inc.

Siemens Product Lifecycle Management Software Inc.
5800 Granite Parkway
Suite 600
Plano, TX. 75024


--------------------
End of Legal Notices
--------------------

--------------
Release Notes:
--------------

Product:        Solid Edge
Version:        100.00.02.07
Date:           03-Dec-2008

This Maintenance Pack can be installed on top of Version:
100.00.00.133 or 100.00.01.07.

Note: Maintenance Packs are all inclusive and can be installed on top of the base
release or any released Maintenance Pack.

--------------------
End of Release Notes
--------------------

-------------------
Installation Notes:
-------------------

After downloading the Maintenance Pack to your machine, dbl click the downloaded
file and the Maintenance Pack will install.

-------------------
End of Installation
-------------------

--------------------------------------------------
This Maintenance Pack addresses the following PRs:
--------------------------------------------------

=====Assembly=====

PR 5863961: Fixed a problem where the first Undo in a sync part cancels current command
PR 6001319: Fixed a problem where assembly features are not showing.
PR 6031604: Fixed a problem where Solid Edge aborts in profile while working w/minimized ribbon
PR 6035914: Fixed a problem where the Tooltips are missing in Mold Tooling
PR 6032872: Fixed a problem where Solid Edge aborts while working on a feature pattern
PR 1668883: Fixed a problem where moving a part causes duplicate occurrences to be created in Edgebar
PR 1685973: Fixed a problem where you cannot locate top level assembly reference planes for angular relationships
PR 2110043: Fixed a problem where Solid Edge aborts when deleting master part of pattern
PR 6045268: Fixed a problem where an assembly is not found when opening a read-only upper-level FOA.
PR 6056820: Fixed a problem where Solid Edge aborts when cursor is moved over failed relationships
PR 6057838: Fixed a problem where Solid Edge aborts when opening a Part from Links dialog using “Open Source”
PR 6059361: Fixed a problem where the angle value field appears on top of the group header bar.
PR 6003473: Fixed a problem where moving faces in assembly results in an Operation Unsuccessful error.
PR 6031381: Fixed a problem where using the persist relation option resulted in a system error
PR 6052910: Fixed a problem where the provided Catia V5 file will not open in Solid Edge.
PR 6030433: Fixed a problem where Solid Edge aborts after modifying a Wire Path name
PR 5980192: Fixed a problem where properties of the supplied Assembly file do not get updated
PR 6022782: Fixed a problem where window controls, zoom area/zoom tool/fit/pan are all dimmed out
PR 6015494: Fixed a problem where physical motion aborts when trying to move a part that has no design body.
PR 6030940: Fixed a problem where adding shaded view to quick access tool bar causes Solid Edge to abort
PR 2098270: Fixed a problem where Solid Edge aborts when clicking white area of Display Configurations
PR 5984045: Fixed a problem where a part does not go back to its original position after Undo.
PR 6026967: Fixed a problem where the previous custom part inherits length of the most recently placed part.
PR 1662218: Fixed a problem where selecting a part to replace in assembly results in a standard parts error
PR 6033504: Fixed a problem where a revolved cutout is incorrectly removing material from the middle of the part
PR 5996010: Fixed a problem where Cam relationships were failing
PR 5728763: Fixed a problem where adding a single constraint to an Adjustable ASM causes other constraint failures

=====Part=====

PR 5782978: Fixed a problem with Zoom Area and Variable table
PR 6020529: Fixed a problem where Solid Edge aborts after selecting a model view in Pathfinder
PR 6033101: Fixed a problem where Solid Edge hangs when saving or closing if ribbon is minimized
PR 2102531: Fixed a problem where creating protrusion with an open profile on a tapered face fails
PR 1681561: Fixed a problem where this pattern circle does not create a connect relationship
PR 6025683: Fixed a problem where a diameter changed via Hole Options is not reflected in the action handle
PR 5771029: Fixed a problem where constraining pattern sketch doesn't work properly.
PR 6034928: Fixed a problem where Solid Edge aborts when undoing a PMI dimension in assembly
PR 1674428: Fixed a problem where populating a member in a large FOP runs out of memory
PR 5988418: Fixed a problem where you cannot select inferred ref planes on a CS when defining local symmetry
PR 6025644: Fixed a problem where a locked group dimension could not be unlocked
PR 1695195: Fixed a problem where you cannot Hide Previous Level when editing a part
PR 6002050: Fixed a problem where you cannot create a perpendicular Helix
PR 6037567: Fixed a problem where the full list of SE tutorials do not display
PR 6053835: Fixed a problem where you cannot ground a hole feature using relate command
PR 6055115: Fixed a problem where separating holes and then changing hole type causes an error
PR 1688195: Fixed a problem where flattening a part results in the wrong cut size
PR 6044788: Fixed a problem where accessing material table causes an abort
PR 2110210: Fixed a problem where Solid Edge aborts when using "Go To" command
PR 1686604: Fixed a problem where editing the supplied part with is not possible
PR 6049456: Fixed a problem where the PromptBar does not remember font size between sessions
PR 6040150: Fixed a problem where Solid Edge Tool Tips do not display properly with Smarteam
PR 5993498: Fixed a problem where shaded highlight on Reference Planes stops working

=====Draft=====

PR 1684163: Fixed a problem where you cannot copy and paste a view that contains coordinate dimension
PR 1535069: Fixed a problem where you are unable to hide overridden edge segments
PR 1644606: Fixed a problem where a Draft of a weldment Assembly is never up to date
PR 1686469: Fixed a problem where Solid Edge aborts when editing a callout with property text
PR 1687099: Fixed a problem where dimensions disappear when views are converted to 2D
PR 2044481: Fixed a problem where you are unable to disconnect connected balloons
PR 6026209: Fixed a problem where you are unable to apply a formula to or using a group dimension between bodies
PR 6038649: Fixed a problem where flow-lines appear to go through the part in an exploded view
PR 6049636: Fixed a problem where Solid Edge aborts when you select the wall of a hole with a hole callout
PR 6051792: Fixed a problem where a Symmetric Diameter Dimension is not correct on a broken view
PR 1672422: Fixed a problem where Solid Edge locks up while adding geometry on the working sheet
PR 2095507: Fixed a problem where Fill is applied to an area outside the selection
PR 1694320: Fixed a problem where Mirror command does not create connect constraints
PR 6042728: Fixed a problem where select set is lost after a reset of a manipulation command
PR 1692306: Fixed a problem where drawing views disappear after opening the file
PR 1682459: Fixed a problem where the Solid Edge line width to ACAD color mapping doesn't work
PR 2108454: Fixed a problem where the supplied Draft file would not open
PR 6026089: Fixed a problem where Copy/Paste is creating an extra working sheets

=====API=====
 
PR 1690493: Fixed a problem where the Custom Edgebar tab does not show up in a legacy addin
PR 1619947: Fixed a problem where a call to SurfaceBoundaries.Add fails with 'type mismatch'.
PR 1691736: Fixed a problem where Class DividedPart does not support Automation from V100
PR 1663220: Added a Block delete API.
PR 1675689: Fixed a problem where 64-bit Solid Edge crashes in Models::AddSweptProtrusion
PR 4007438: Fixed a problem where you were unable to create previews under properties via automation
PR 1693313: Added the ability to add both a bitmap and text on UI buttons created by addins

=====Insight=====
 
PR 5991609: Fixed a problem where you were unable to run View and Markup in 64-bit Solid Edge 2D Drafting (M)
PR 6045318: Fixed a problem where LCA will not change “In work” back to “Available”
PR 1687267: Fixed a problem where changing display configurations of subassembly will cause an abort
PR 6048198: Fixed a problem where you are not able to select a zone on the File -> Open dialog

---
End
---