Solid Edge ST7 SDK
Solid Edge ST MP6 - Readme

--------------
Legal Notices
--------------
©2009 Siemens Product Lifecycle Management Software Inc.

All Rights Reserved
Software, file formats, and audiovisual displays may be used pursuant to the
applicable Software License Agreement and contain confidential and proprietary
information of Siemens Product Lifecycle Management Software Inc.; which is
protected by copyright and trade secret law. Such materials may not be reproduced
or transferred to other documents or used or disclosed to others for manufacturing
or for any other purpose except as specifically authorized within the terms of the
Software License Agreement, or as specifically authorized in writing by Siemens
Product Lifecycle Management Software Inc.

Siemens Product Lifecycle Management Software Inc.
5800 Granite Parkway
Suite 600
Plano, TX. 75024


--------------------
End of Legal Notices
--------------------

--------------
Release Notes:
--------------

Product:        Solid Edge
Version:        100.00.06.03
Date:           15-Apr-2009

This Maintenance Pack can be installed on top of Versions:
100.00.00.133, 100.00.01.07, 100.00.02.07, 100.00.03.03, 100.00.04.04,
100.00.05.04

Note: Maintenance Packs are all inclusive and can be installed on top of the base
release or any released Maintenance Pack.

--------------------
End of Release Notes
--------------------

-------------------
Installation Notes:
-------------------

After downloading the Maintenance Pack to your machine, dbl click the downloaded
file and the Maintenance Pack will install.

-------------------
End of Installation
-------------------

--------------------------------------------------
This Maintenance Pack addresses the following PRs:
--------------------------------------------------

=====Assembly=====

PR 6097501: Weld features failed each time the weldment assembly file is opened
PR 6101187: SAT File Fails to Open
PR 1713572: Reference Feature step selecting faces instead of entire feature
PR 6069017: Assembly aborts during open
PR 6111867: Unable to select individual sketch items when IPA into sub-assembly
PR 6119191: Solid Edge hangs when opening this draft file
PR 6124646: When translating Catia assemblies, curves, surf's, and solids are lumped together

=====Part/Profile/Sheet Metal=====

PR 6101666: Running quickly out of memory on a 64 bit machine (SE 32 bit)
PR 5983131: EMS Translator fails to import any file
PR 6119137: Solid Edge (French) crashes when moving cursor over Quickbar Single/All button
PR 2118948: File hangs at the splash screen
PR 6118550: Mouse Scroll wheel on edit should adjust value of a round by 5% of initial value

=====Draft=====

PR 6123655: can't extract bodies from MDT files
PR 1643072: Unable to save a PDF file from Solid Edge to a path with a comma
PR 1694065: A scaled dimension is no longer scaled after being re-attached
PR 1711103: Solid Edge will export elliptical arcs as splines

===API===

PR 6098711: SelectSetChanged events not being fired properly from select tool in Synchronous

===Insight/View & Markup===

PR 1720400: Cannot open Parasolid files in View and markup with Hebrew filenames

=====Embedded Client=====

PR 1678740: The Dataset Keep Limit is ignored
PR 1691073: if the query from Solid Edge contains an Integer LoV the search results are empty
PR 6023631: When an assembly is viewed via PSE the assemblies JT override file is not used
PR 6125319: JT overrides created by SEEC do not contain BREP data as specified in the ini file

---
End
---