--------------
Legal Notices
--------------
©2009 Siemens Product Lifecycle Management Software Inc.
All Rights Reserved
Software, file formats, and audiovisual displays may be used pursuant to the
applicable Software License Agreement and contain confidential and proprietary
information of Siemens Product Lifecycle Management Software Inc.; which is
protected by copyright and trade secret law. Such materials may not be reproduced
or transferred to other documents or used or disclosed to others for manufacturing
or for any other purpose except as specifically authorized within the terms of the
Software License Agreement, or as specifically authorized in writing by Siemens
Product Lifecycle Management Software Inc.
Siemens Product Lifecycle Management Software Inc.
5800 Granite Parkway
Suite 600
Plano, TX. 75024
--------------------
End of Legal Notices
--------------------
--------------
Release Notes:
--------------
Product: Solid Edge
Version: 100.00.07.04
Date: 20-May-2009
This Maintenance Pack can be installed on top of Versions:
100.00.00.133, 100.00.01.07, 100.00.02.07, 100.00.03.03, 100.00.04.04,
100.00.05.04, 100.00.06.03
Note: Maintenance Packs are all inclusive and can be installed on top of the base
release or any released Maintenance Pack.
--------------------
End of Release Notes
--------------------
-------------------
Installation Notes:
-------------------
After downloading the Maintenance Pack to your machine, dbl click the downloaded
file and the Maintenance Pack will install.
-------------------
End of Installation
-------------------
--------------------------------------------------
This Maintenance Pack addresses the following PRs:
--------------------------------------------------
=====Assembly=====
PR 1673892: Selecting new base plane results in wrong orientation
PR 1706516: Groove Weld missing in View & Markup
PR 6031625: Solid Edge crashes when converting this assembly to a Synchronous Assembly
PR 6086371: Solid Edge crashes when manipulating timeline pointer in the animation editor
PR 6109170: Frequent crashes in ST, fixes added based on info from the crashlogs
PR 6124646: Curves, Surfaces, and Solids are lumped together when importing a Catia file
PR 1698824: Scroll to Part is not working correctly within a patterned sub-assembly
PR 1707765: Unable to create small spur gear in Engineering Reference
PR 5993959: Cannot generate Insight managed Standard Parts on 64bit client
PR 6129398: Activating a part while moving another causes activated part to disappear
PR 1686303: Variable values do not update if the linked excel file is missing
PR 6144280: Virtual Component support commands are not enabled with Foundation
PR 6144967: Can't Copy a Released file while IPA
PR 2072031: Solid Edge is consuming more USER and GDI objects than needed
PR 6144353: After creating a discrete list in the variable table, accessing the drop down list causes an abort
=====Part/Profile/Sheet Metal=====
PR 1715352: Wrong hole information in hole table
PR 6112485: Dynamic Edit of Rounds with the scroll wheel doesn't work correct for synchronous part
PR 6118906: Unable to return to initial value when using mouse Scroll Wheel
PR 6152305: Setting a value to 0 with the scroll wheel does not allow you to change it back up 5%
PR 2112417: Can't select Datum Target and Datum Point with Move Dimension command
PR 6138584: Failures adding constraints to sketches
PR 1705359: Drawing views showing out of date, when no updates are needed
PR 6145040: Variable Table crash
PR 1714042: In a Synchronous part the position of patterned holes do not move correctly
PR 1714050: Command p= base plane seems not to work, when pasting a sketch
PR 1720942: Performance issue when saving a file after pasting elements from draft
PR 1714037: Solid Edge crashes with SpaceNavigator
=====Draft=====
PR 1687315: Graphical line type selection in Layer and Attribute mapping not correct
PR 1680872: Modify balloon command does not set focus to balloon text
PR 6126396: Draft aborts passing over lines with Edge Painter
PR 1703321: Invisible Block labels are exported to DWG
PR 1703366: Block Label angle is ignored on export to DWG
PR 6147727: You cannot delete a balloon from graphic screen in the provided Synchronous part
PR 1712799: Viewer data is incorrect
PR 1724661: unable to open the provided Assembly file
PR 6140083: Parts list is showing several parts that are not included in the List Control tab
===API===
PR 6081122: Added Synchronous support in sereader.dll, sefacet.dll
PR 2091452: Incorrect transform for highlight thru automation
PR 1711881: Properties from Ideas JT are not going in sole edge sub assemblies
PR 2119076: "ConstructionModel.Features" object is not obtained in the synchronous mode
PR 1681758: Added additional support for adding multiple tabs and groups on a tab of the command ribbon, added support for check and radio buttons
===Insight/View & Markup===
PR 1716735: Revision Manger generates wrong links to FOA/Variables
PR 1727458: Can't replace Sync parts with Traditional parts in Revision Manager
=====Embedded Client=====
PR 6125319: JT over-rides created by SEEC do not contain BREP data as specified in the ini
PR 6067211: FMS failures during AddToTeamcenter for the submitted dataset
PR 6138857: AddToTeamcenter does not complete a resume import with Tc8.0.01
PR 1680912: The quantity of a non-graphical part is DELETED
PR 6049892: SEEC structure editor will crash when switching between parts list and exploded
PR 6143758: SEEC:AtT: Manage restart after system power failure
PR 1722104: "Save as translated" does not work with model/draft file combinations
PR 6033016: SEEC cache should not be case sensitive
PR 6150125: SEEC TAL Update to Tc2007.1.7 Client Framework
---
End
---