Application | Returns the active application object. |
AttributeSets | Returns the AttributeSets collection object for the referenced object. |
IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. |
Parent | Returns the parent object for the referenced object. |
Radius | Returns the radius of the referenced object. |
SweepAngle | Sets and returns the angle, in radians, at which the arc ends along a circle or ellipse with regard to the major axis of the referenced object. |
Type | Specifies the type of the object being referenced. |