Solid Edge Assembly Type Library
SweepAngle Property
Collapse All
Expand All
Solid Edge Assembly Type Library
>
ArcSegment Object
: SweepAngle Property
Description
Sets and returns the angle, in radians, at which the arc ends along a circle or ellipse with regard to the major axis of the referenced object.
Property type
Read-write property
Syntax
Visual Basic
Public Property SweepAngle As Double
Remarks
The Start Angle and Sweep Angle combine to define the start and end of an arc along a circle or ellipse.
See Also
ArcSegment Object
|
ArcSegment Members