Solid Edge Assembly Type Library : AssemblyCopy Object |
ChangeSource | This method needs to be called only if the caller wants to change the parent assembly filename. In which case, we need to know what components need to be included and/or excluded. |
ComponentSettings | To Edit an existing AssemblyCopy (IAC Mirror), the caller first needs to get the definition of the AssemblyCopy via GetDefinition() that returns the included/excluded occurrences, output occurrences(not necessary for edit) and Actions array , AdjustPlane Array and userEnums, whether the input occurrence is included or excluded in the definition and the options chosen for each occurrence. |
GetDefinition | |
GetMultibodyDefinition | |
Update |
AddNewComponentsOnUpdate | |
Application | |
AssemblyCopyType | |
CoordinateSystem | |
IncludeAssemblyFeatures | |
IsFrozen | |
IsOutOfDate | |
MirrorPlane | |
Name | |
Parent | |
SourceDocument | |
SourceFilename | |
Status |