Solid Edge Assembly Type Library : Bundle Object |
CreatePhysicalConductor | |
Delete | Deletes the referenced object. |
DeletePhysicalConductor | |
Edit | |
GetAdders | |
GetAllPaths | |
GetConductors | |
GetEndPoints | This method returns the start and end points of the referenced object. |
GetOuterConductors | |
GetPaths | |
GetTopMostConductors | |
Remove | |
SetAdders |
Application | Returns the active application object. |
AssemblyProperty | Returns the AssemblyProperty object used to store path attributes for the referenced object. |
AttributeSets | Returns the AttributeSets collection object for the referenced object. |
Color | This read-write property sets or returns the color in which the active object is drawn. The color is stored as a long integer and is created with the RGB function (red, green, and blue color intensities) or as an integer between 0 and 16 that represents standard colors. |
CutLength | |
Description | |
IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. |
LinearDensity | |
Mass | |
MinimumBendRadius | |
Name | Returns the name of the referenced object. |
OuterDiameter | Sets and returns the outer diameter of the referenced object. |
Parent | Returns the parent object for the referenced object. |
PartNumber | |
TrueLength | |
Type | Specifies the type of the object being referenced. |
UseGlobalAdders | |
Visible | Specifies whether or not the referenced object is displayed to the screen. |