Solid Edge Assembly Type Library
StartDerivativeMagnitude Property
Collapse All
Expand All
Solid Edge Assembly Type Library
>
CurveSegment Object
: StartDerivativeMagnitude Property
Description
Sets and returns the start derivative magnitude.
Property type
Read-write property
Syntax
Visual Basic
Public Property StartDerivativeMagnitude As Double
Remarks
Sets and returns the direction and degree of influence of the b-spline curve on the curvature of the curve at the start point for the referenced CurveSegment object. Valid range is -1 to 1.
See Also
CurveSegment Object
|
CurveSegment Members