Solid Edge Assembly Type Library
Index Property
Description
Returns the numeric index for the active object.
Property type
Read-only property
Syntax
Visual Basic
Public Property Index As Long
Remarks
This index is the sequence that the object holds in its collection object (as held by the parent).
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgeAssembly.AssemblyDocument
    Dim objRelations3D As SolidEdgeAssembly.Relations3d
    Dim objGround As SolidEdgeAssembly.GroundRelation3d
    Dim lngIndex As Long
    Const TESTFILE = "T:\vbtests\testcases\Sample.asm"
    ' Report errors
    Const PI = 3.14159265358979
    ' Create/get the application with specific settings
    On Error Resume Next
    Set objApp = GetObject(, "SolidEdge.Application")
    If Err Then
        Err.Clear
        Set objApp = CreateObject("SolidEdge.Application")
        Set objDoc = objApp.Documents.Add("SolidEdge.AssemblyDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    Call objDoc.Close
    ' opening an existing assembly document
    Set objDoc = objApp.Documents.Open(TESTFILE)
    ' getting the Relations3D object from the assembly document
    Set objRelations3D = objDoc.Relations3d
    ' getting the Ground Relation object
    Set objGround = objRelations3D.Item(1)
    ' getting the index of the ground relation in the collection object
    lngIndex = objGround.Index
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objRelations3D = Nothing
    Set objGround = Nothing
End Sub
See Also

GroundRelation3d Object  | GroundRelation3d Members