Solid Edge Assembly Type Library
IsAttributeSetPresent Property
Description
Returns True if a specified Attribute Set exists on the referenced object.
Property type
Read-only property
Syntax
Visual Basic
Public Property IsAttributeSetPresent( _
   ByVal Name As String _
) As Boolean
Parameters
Name
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgeAssembly.AssemblyDocument
    Dim objRelations3D As SolidEdgeAssembly.Relations3d
    Dim objGround As SolidEdgeAssembly.GroundRelation3d
    Dim objAttributeSets As Object
    Const TESTFILE = "T:\vbtests\testcases\Sample.asm"
    Dim bAttribSetPresent As Boolean
    ' Report errors
    Const PI = 3.14159265358979
    ' Create/get the application with specific settings
    On Error Resume Next
    Set objApp = GetObject(, "SolidEdge.Application")
    If Err Then
        Err.Clear
        Set objApp = CreateObject("SolidEdge.Application")
        Set objDoc = objApp.Documents.Add("SolidEdge.AssemblyDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    Call objDoc.Close
    ' opening an existing assembly document
    Set objDoc = objApp.Documents.Open(TESTFILE)
    ' getting the Relations3D object from the assembly document
    Set objRelations3D = objDoc.Relations3d
    ' getting the Ground Relation object
    Set objGround = objRelations3D.Item(1)
    'Get the AttributeSets collection object
    Set objAttributeSets = objGround.AttributeSets
    'Create an AttributeSet
    objAttributeSets.Add "MyAttribSet"
    'Check for the presence of the AttributeSet
    bAttribSetPresent = objGround.IsAttributeSetPresent("MyAttribSet")
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objRelations3D = Nothing
    Set objGround = Nothing
    Set objAttributeSets = Nothing
End Sub
See Also

GroundRelation3d Object  | GroundRelation3d Members