Solid Edge Assembly Type Library : Occurrence Object |
AddAlternateComponent | This method adds an alternate component to the specified Occurrence object. |
CaptureRelationships | This method takes an array of relationships for the occurrence to capture and captures the relationships. |
ClearCapturedRelationships | This method clears the relationships that have already been captured for the occurrence. |
CreateTopologyReference | Creates a TopologyReference object that points to a topological (G&T) element contained within the definition of the referenced Occurrence or SubOccurrence object. |
CreateTopologyReferenceToBodyOverride | |
Delete | Deletes the referenced object. |
DeleteHoleLocation | Deletes the construction surfaces from the frame. |
FileMissing | This method will check if the particular file is missing or not. |
GetAdjustablePart | Returns the adjustable part object. |
GetAllAlternateComponents | This method returns all alternate components for the specified Occurrence object. |
GetBodyInversionMatrix | |
GetExplodeMatrix | |
GetFaceStyle2 | This method specifies whether user style preferences are returned for the referenced object. |
GetInterpartDrivenOccurrences | |
GetInterpartDrivingOccurrences | |
GetMatrix | Returns the transformation matrix for the referenced occurrence. |
GetOrigin | Returns the origin for the referenced object. |
GetReferenceKey | Returns a reference key for the referenced object. |
GetSimplifiedBodies | |
GetSimplifiedBodies2 | Returns an array of bodies and an array of transforms for those bodies contained in the simplified assembly model of the occurrence. |
GetTransform | Returns the current location and orientation of the referenced object. |
GetTube | This method returns the Tube object for the referenced Occurrence object. |
IsAlternateComponent | This Boolean method returns whether the specified Occurrence object is an alternate component. |
IsTube | Returns True if the referenced Occurrence is a Tube, false if it is not. |
MakeAdjustablePart | Makes the part as adjustable. Part file must be adjustable. |
MakeWritable | Sets the referenced Occurrence or subassembly to allow changes to be written to the file. |
Move | Moves the referenced object. |
PutMatrix | Sets the transformation matrix for the referenced occurrence. |
PutOrigin | Sets a new origin for the referenced object. |
PutTransform | Sets the current location and orientation of the referenced object. |
Range | |
RecheckMissingFile | Returns a bool value if the file is found which was previously missing |
RemoveAllAlternateComponents | This method removes all alternate components from the specified Occurrence object. |
RemoveAlternateComponent | This method removes an alternate component from the specified Occurrence object. |
RemoveOverrideBody | This method removes the dumb override body that exists on the assembly occurrence. |
Replace | Replaces the referenced file with a new file. |
ResetName | |
RetrieveHoleLocation | Retrieves the construction surfaces representing the hole locations from the cross section component file. These surfaces can be used to create holes as per the standard at appropriate locations in the frames. |
Rotate | Rotates the referenced object. |
Select | Selects the referenced object in the active window. |
SwapFamilyMember | Swaps the current family member with one you specify. |
Activate | Makes the referenced object the active one. |
Adjustable | Specifies whether the referenced object is adjustable. |
Application | Returns the active application object. |
AttributeSets | Returns the AttributeSets collection object for the referenced object. |
Body | Returns the Body object for the referenced object. |
CoordinateSystemsVisible | |
DisplayAsLastSaved | Specifies whether the last saved display is visible in the referenced object. |
DisplayAsReference | Displays the specified parts as reference parts. |
DisplayCenterline | |
DisplayConstrCurves | Specifies whether construction curves are visible in the referenced object. |
DisplayConstructions | Specifies whether constructions are visible in the referenced object. |
DisplayCoordinateSystems | Specifies whether coordinate systems are visible in the referenced object. |
DisplayInDrawings | Controls whether or not the referenced occurrence or assembly is visible in the draft environment. |
DisplayInSubAssembly | Specifies whether the referenced occurrence is shown or hidden when this assembly is inserted into another assembly. |
DisplayReferenceAxes | Specifies whether reference axes are visible in the referenced object. |
DisplayReferencePlanes | Specifies whether reference planes are visible in the referenced object. |
DisplaySketches | Specifies whether sketches are visible in the referenced object. |
FaceStyle | Sets and returns the FaceStyle object for the referenced occurrence. |
HasBodyOverride | Creation of an assembly feature, for example, on an Occurrence of an assembly results in an override body being created for the Occurrence in the context of the assembly. Solid Edge uses the override body in place of the body from the Occurrence document in the assembly for display, interference analysis etc. |
HasNongraphicQuantity | Returns True if the referenced Occurrence has a non-graphic quantity numeric value, false if it does not. |
HasUserDefinedName | |
IncludeInBom | Controls whether or not the referenced occurrence is included in reports. |
IncludeInInterference | |
IncludeInPhysicalProperties | Controls whether or not the referenced occurrence is included in physical property calculations. |
Index | Returns the numeric index for the active object. |
IsAdjustablePart | Tests whether part is adjustable part. |
IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. |
IsCopy | |
IsFamilyOfAssembly | This read-only Boolean property specifies whether or not the referenced Occurrence object is a family of assembly. |
IsFamilyOfParts | Returns if the occurence is a family of parts i.e a member or a master |
IsFastenerSystemItem | |
IsForeign | Specifies whether or not the referenced occurrence orginated from an application other than Solid Edge. |
IsNongraphic | Returns True if the referenced Occurrence is non-graphic, false if it is not. |
IsPatterned | |
IsPatternItem | |
IsPipeFitting | |
IsPipeSegment | |
IsStructuralFrameItem | |
IsWire | |
ItemNumber | |
Locatable | Sets and returns the referenced object's locatable state. |
Name | Returns the name of the referenced object. |
NodeType | |
NongraphicDescription | Returns the non-graphic quantity description if one exists. |
NongraphicPrecision | Returns the number of digits of precision to use to display the non-graphic quantity numeric value if one exists. |
NongraphicQuantity | Gets or sets the non-graphic quantity numeric value if one exists. |
OccurrenceDocument | Returns the OccurrenceDocument object for the active occurrence. |
OccurrenceFileName | Returns the name of the data file for the OccurrenceDocument object of the active occurrence. |
Parent | Returns the parent object for the referenced object. |
Quantity | Returns the number of occurrences of the referenced object. |
ReferenceOnly | Returns the 'reference-only' state of the active occurrence. |
ReferencePlanesVisible | |
Relations3d | Returns a collection of Relations3d objects for the referenced Part. |
SketchesVisible | |
Status | Returns the status (a member of the OccurrenceStatusConstants constant set) of the referenced Occurrence. |
Style | Returns the style for the referenced object. |
Subassembly | Returns True if the referenced object is a subassembly. |
SubassemblyBodies | |
SubOccurrences | Returns the Suboccurrences collection object for the referenced Occurrence. |
TopLevelDocument | Returns the toplevel AssemblyDocument object. |
Type | A member of the ObjectType constant set. |
UseSimplified | Gets or sets whether the referenced leafpart Occurrence is using a simplified model. |
Visible | Controls the display of the referenced object. |