Solid Edge Assembly Type Library
GetMatrix Method
Returns the 4x4 array that specifies the position and orientation of the part. This is a single-dimension Double array that contains 16 elements.
Description
Returns the transformation matrix for the referenced occurrence.
Syntax
Visual Basic
Public Sub GetMatrix( _
   ByRef Matrix() As Double _
) 
Parameters
Matrix
Returns the 4x4 array that specifies the position and orientation of the part. This is a single-dimension Double array that contains 16 elements.
Remarks
This matrix defines the current position and orientation of the object.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgeAssembly.AssemblyDocument
    Dim objPart As SolidEdgeAssembly.Occurrence
    Dim dblMatrix() As Double
    Const TESTFILE = "T:\vbtests\testcases\Sample.asm"
    ' Report errors
    Const PI = 3.14159265358979
    ' Create/get the application with specific settings
    On Error Resume Next
    Set objApp = GetObject(, "SolidEdge.Application")
    If Err Then
        Err.Clear
        Set objApp = CreateObject("SolidEdge.Application")
        Set objDoc = objApp.Documents.Add("SolidEdge.AssemblyDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    Call objDoc.Close
    ' opening an existing assembly file
    Set objDoc = objApp.Documents.Open(TESTFILE)
    ' getting a part in the assembly
    Set objPart = objDoc.Occurrences.Item(1)
    ' getting the matrix associated with the part
    Call objPart.GetMatrix(matrix:=dblMatrix)
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objPart = Nothing
End Sub
See Also

Occurrence Object  | Occurrence Members