Private Sub Form_Load()
Dim objApp As SolidEdgeFramework.Application
Dim objDoc As SolidEdgeAssembly.AssemblyDocument
Dim objPart As SolidEdgeAssembly.Occurrence
Dim dblDeltaX As Double
Dim dblDeltaY As Double
Dim dblDeltaZ As Double
Dim dblOriginX As Double
Dim dblOriginY As Double
Dim dblOriginZ As Double
Const TESTFILE = "T:\vbtests\testcases\cube.par"
' Report errors
Const PI = 3.14159265358979
' Create/get the application with specific settings
On Error Resume Next
Set objApp = GetObject(, "SolidEdge.Application")
If Err Then
Err.Clear
Set objApp = CreateObject("SolidEdge.Application")
Set objDoc = objApp.Documents.Add("SolidEdge.AssemblyDocument")
objApp.Visible = True
Else
Set objDoc = objApp.ActiveDocument
End If
' adding a part document to the assembly document
Set objPart = objDoc.Occurrences.AddByFilename(OccurrenceFileName:=TESTFILE)
' moving the part in the assembly
dblDeltaX = 0.05
dblDeltaY = 0.075
dblDeltaZ = 0.1
Call objPart.Move(deltaX:=dblDeltaX, deltaY:=dblDeltaY, deltaZ:=dblDeltaZ)
' USER DISPLAY
' Release objects
Set objApp = Nothing
Set objDoc = Nothing
Set objPart = Nothing
End Sub